I currently have an Arduino UNO board that I use to program an ATTiny85. I just recently bought a Grove Base Shield for my Arduino to start modulizing everything I do with it. Is there some type of Grove module I can get to work with the Base Shield? One that would allow me to program the ATTiny85 and/or other ICs?
Hi there~
Please see below replies. Hope it helps.
- All the grove modules work with Base shield v2.0.
- For use the uno to program the ATTiny85 , you can refer to below link.
<LINK_TEXT text=“https://create.arduino.cc/projecthub/ar … uno-afb829”>https://create.arduino.cc/projecthub/arjun/programming-attiny85-with-arduino-uno-afb829</LINK_TEXT>