Grove AI vision - Install tensorflow for yolov5-swift error

I’m looking for a way to train a custom model for Grove AI vision to detect vehicles (car/motorbike/bus) and I have followed this guide. But when I install the required packages, it shows errors that cannot find the suitable version.

Cloning into 'yolov5-swift'...
remote: Enumerating objects: 9409, done.
remote: Total 9409 (delta 0), reused 0 (delta 0), pack-reused 9409 (from 1)
Receiving objects: 100% (9409/9409), 22.61 MiB | 7.55 MiB/s, done.
Resolving deltas: 100% (6269/6269), done.
/content/yolov5-swift
ERROR: Could not find a version that satisfies the requirement tensorflow==2.9.0 (from versions: 2.12.0rc0, 2.12.0rc1, 2.12.0, 2.12.1, 2.13.0rc0, 2.13.0rc1, 2.13.0rc2, 2.13.0, 2.13.1, 2.14.0rc0, 2.14.0rc1, 2.14.0, 2.14.1, 2.15.0rc0, 2.15.0rc1, 2.15.0, 2.15.0.post1, 2.15.1, 2.16.0rc0, 2.16.1, 2.16.2, 2.17.0rc0, 2.17.0rc1, 2.17.0, 2.17.1, 2.18.0rc0, 2.18.0rc1, 2.18.0rc2, 2.18.0, 2.18.1, 2.19.0rc0, 2.19.0)
ERROR: No matching distribution found for tensorflow==2.9.0

Does anyone ever train a custom model could help me?
Is the Grove AI module able to detect multiple objects or only one object, since most models on Sensecraft are for one object detection only?

Hi, try executing the following snippet at the very beginning of the Colab first:

%%bash
MINICONDA_INSTALLER_SCRIPT=Miniconda3-4.5.4-Linux-x86_64.sh
MINICONDA_PREFIX=/usr/local
wget https://repo.continuum.io/miniconda/$MINICONDA_INSTALLER_SCRIPT
chmod +x $MINICONDA_INSTALLER_SCRIPT
./$MINICONDA_INSTALLER_SCRIPT -b -f -p $MINICONDA_PREFIX

conda install --channel defaults conda python=3.8 --yes
conda update --channel defaults --all --yes

thank you, you’ve save my project