I’ve already upgraded to the current version, which adds Watcher support. But it still doesn’t work with my boards here. I attached the screens so you can see the inconsistency. The board is connected to wifi, to the MQTT server, it receives messages, but the SenseCraft integration does not detect it.
My suspicion was the inconsistency in the customer names, but after testing, the problem persists. I also analyzed the source code of the AT firmware for ESP32 and did not find anything in it that would cause this problem.