Groove Vision AI V2 - I can't get Homeassistant to work

In step 11 of the wiki - Connecting to Home Assistant | Seeed Studio Wiki, I can’t get Groove Vision AI V2 to be found by Homeassistant. Looking at the EMQX Logs, I notice that the board connects with MQTT. But in step by step, I can’t make the connection. Timeout error occurs.

The system does not automatically find my device, and manual configuration is required. In this case, when filling out the SETUP MQTT SERVER form with my server information, I cannot connect through setup.

MQTT connection timeout

EMQX - Connection Info

|Status|Connected|
|Node|[email protected]|
|Client ID| grove_vision_ai_v2
|Username| myuser
|Protocol| MQTT v3.1.1|
|IP Address| myGrooveIpAddress:57773|
|Keepalive| 15|
|Clean Session|true|
|Bridge|false|
|Connected At|2024-05-11 13:22:39|

Session Info

|Session Expiry Interval|0|
|Created At|2024-05-11 13:22:39|
|Heap Size|2586 bytes|
|Subscriptions|1/infinity|
|Message Queue|0/1000View Message|
|Inflight|0/32View Message|
|QoS 2 Message Receive Queue|0/100|

Same issue. Used the mqtt2uart example and get wifi and mqtt connected. EQMX detects the board, but the alleged integration not… Exactly one month, and this still not working and there is no support.

I’m sorry I’m late. I will test it for your situation. We apologize for the inconvenience. We’ll be sure to contact you here as soon as we have the results.

Another hint is, when SenseCraft extension try to integrate my Groove Vision AI V2, the name header start with grove_vision_ai_we2_uniqueid and not grove_vision_ai_v2_uniqueid.

If you arrived at this topic after trying unsuccessfully to configure your Groove Vision Ai V2 to work with Home Assistant, first take a look at the date of previous messages and the response time between them.

Hi there,
Sounds like an Island… LOL, I’m about to embark on the same journey, HA with Gove Vision Ai V2 and a coral AI M2 e-key version all in an Intel NUC as host machine. It’s an I5 so plenty of juice for the squeeze also some IP cameras too. I anticipate some hurdles.
GL :slight_smile: PJ
:v:

In file strings.json, the name of the board is typed wrong.
grove_vision_ai_we2 instead of grove_vision_ai_v2

Proposed correction, but I will try it mannualy sometime.

I’ve already upgraded to the current version, which adds Watcher support. But it still doesn’t work with my boards here. I attached the screens so you can see the inconsistency. The board is connected to wifi, to the MQTT server, it receives messages, but the SenseCraft integration does not detect it.

My suspicion was the inconsistency in the customer names, but after testing, the problem persists. I also analyzed the source code of the AT firmware for ESP32 and did not find anything in it that would cause this problem.




Are you still here? I keep trying to get the Home Assistant integration to work, but it doesn’t. I saw that you updated to support the future Watcher, but it still doesn’t work on Grove Vision AI V2 and it’s possible that the problem with this integration will continue like this.

Something is wrong. Either the tutorial has a missing step, or the integration does not work as advertised.

or cliffs… :hole: :person_with_white_cane:
HA is a moving target anyway , looks like this will make it even more elusive. I can only wish they slow down and clean up what they have, well I can hope anyway. They need like 10 more engineers IMO. :crossed_fingers:

Just to confirm, which device’s IP address is 192.168.15.29?

This address is for my HomeAssistant server, an Orange Pi 3 LTS.

Hello

same problem here. cant add to HA dont know why. everything same as your situation. is there any solution for you? thanks.