Why i cant run simple coding of gps neo 6m sensor with esp32c3 xiao? help me
I think the problem is with the hardware serial…
different hardware uses serial differently
FYI
This is from my archive, havent tested in a while, some custom edits but may give you some ideas if you review the code
#include <TinyGPSPlus.h>
#include <SoftwareSerial.h>
/*
This sample code demonstrates just about every built-in operation of TinyGPSPlus (TinyGPSPlus).
It requires the use of SoftwareSerial, and assumes that you have a
9600-baud serial GPS device hooked up on pins 7(rx) and 6(tx).
*/
static const int RXPin = 7, TXPin = 6;
static const uint32_t GPSBaud = 9600;
// The TinyGPSPlus object
TinyGPSPlus gps;
// The serial connection to the GPS device
SoftwareSerial ss(RXPin, TXPin);
// For stats that happen every 5 seconds
unsigned long last = 0UL;
void setup()
{
Serial.begin(9600);
ss.begin(GPSBaud);
Serial.println(F("KitchenSink.ino"));
Serial.println(F("Demonstrating nearly every feature of TinyGPSPlus"));
Serial.print(F("Testing TinyGPSPlus library v. ")); Serial.println(TinyGPSPlus::libraryVersion());
Serial.println(F("by Mikal Hart"));
Serial.println();
}
void loop()
{
// Dispatch incoming characters
while (ss.available() > 0)
gps.encode(ss.read());
if (gps.location.isUpdated())
{
Serial.print(F("LOCATION Fix Age="));
Serial.print(gps.location.age());
Serial.print(F("ms Raw Lat="));
Serial.print(gps.location.rawLat().negative ? "-" : "+");
Serial.print(gps.location.rawLat().deg);
Serial.print("[+");
Serial.print(gps.location.rawLat().billionths);
Serial.print(F(" billionths], Raw Long="));
Serial.print(gps.location.rawLng().negative ? "-" : "+");
Serial.print(gps.location.rawLng().deg);
Serial.print("[+");
Serial.print(gps.location.rawLng().billionths);
Serial.print(F(" billionths], Lat="));
Serial.print(gps.location.lat(), 6);
Serial.print(F(" Long="));
Serial.println(gps.location.lng(), 6);
}
else if (gps.date.isUpdated())
{
Serial.print(F("DATE Fix Age="));
Serial.print(gps.date.age());
Serial.print(F("ms Raw="));
Serial.print(gps.date.value());
Serial.print(F(" Year="));
Serial.print(gps.date.year());
Serial.print(F(" Month="));
Serial.print(gps.date.month());
Serial.print(F(" Day="));
Serial.println(gps.date.day());
}
else if (gps.time.isUpdated())
{
Serial.print(F("TIME Fix Age="));
Serial.print(gps.time.age());
Serial.print(F("ms Raw="));
Serial.print(gps.time.value());
Serial.print(F(" Hour="));
Serial.print(gps.time.hour());
Serial.print(F(" Minute="));
Serial.print(gps.time.minute());
Serial.print(F(" Second="));
Serial.print(gps.time.second());
Serial.print(F(" Hundredths="));
Serial.println(gps.time.centisecond());
}
else if (gps.speed.isUpdated())
{
Serial.print(F("SPEED Fix Age="));
Serial.print(gps.speed.age());
Serial.print(F("ms Raw="));
Serial.print(gps.speed.value());
Serial.print(F(" Knots="));
Serial.print(gps.speed.knots());
Serial.print(F(" MPH="));
Serial.print(gps.speed.mph());
Serial.print(F(" m/s="));
Serial.print(gps.speed.mps());
Serial.print(F(" km/h="));
Serial.println(gps.speed.kmph());
}
else if (gps.course.isUpdated())
{
Serial.print(F("COURSE Fix Age="));
Serial.print(gps.course.age());
Serial.print(F("ms Raw="));
Serial.print(gps.course.value());
Serial.print(F(" Deg="));
Serial.println(gps.course.deg());
}
else if (gps.altitude.isUpdated())
{
Serial.print(F("ALTITUDE Fix Age="));
Serial.print(gps.altitude.age());
Serial.print(F("ms Raw="));
Serial.print(gps.altitude.value());
Serial.print(F(" Meters="));
Serial.print(gps.altitude.meters());
Serial.print(F(" Miles="));
Serial.print(gps.altitude.miles());
Serial.print(F(" KM="));
Serial.print(gps.altitude.kilometers());
Serial.print(F(" Feet="));
Serial.println(gps.altitude.feet());
}
else if (gps.satellites.isUpdated())
{
Serial.print(F("SATELLITES Fix Age="));
Serial.print(gps.satellites.age());
Serial.print(F("ms Value="));
Serial.println(gps.satellites.value());
}
else if (gps.hdop.isUpdated())
{
Serial.print(F("HDOP Fix Age="));
Serial.print(gps.hdop.age());
Serial.print(F("ms raw="));
Serial.print(gps.hdop.value());
Serial.print(F(" hdop="));
Serial.println(gps.hdop.hdop());
}
else if (millis() - last > 5000)
{
Serial.println();
if (gps.location.isValid())
{
static const double LONDON_LAT = 51.508131, LONDON_LON = -0.128002;
double distanceToLondon =
TinyGPSPlus::distanceBetween(
gps.location.lat(),
gps.location.lng(),
LONDON_LAT,
LONDON_LON);
double courseToLondon =
TinyGPSPlus::courseTo(
gps.location.lat(),
gps.location.lng(),
LONDON_LAT,
LONDON_LON);
Serial.print(F("LONDON Distance="));
Serial.print(distanceToLondon/1000, 6);
Serial.print(F(" km Course-to="));
Serial.print(courseToLondon, 6);
Serial.print(F(" degrees ["));
Serial.print(TinyGPSPlus::cardinal(courseToLondon));
Serial.println(F("]"));
}
Serial.print(F("DIAGS Chars="));
Serial.print(gps.charsProcessed());
Serial.print(F(" Sentences-with-Fix="));
Serial.print(gps.sentencesWithFix());
Serial.print(F(" Failed-checksum="));
Serial.print(gps.failedChecksum());
Serial.print(F(" Passed-checksum="));
Serial.println(gps.passedChecksum());
if (gps.charsProcessed() < 10)
Serial.println(F("WARNING: No GPS data. Check wiring."));
last = millis();
Serial.println();
}
}
Hi there,
Not sure if it will help you , but I have a demo with the Xiao nrf52 here working , may help
HTH
GL
PJ
but it say i cant use software serial? is there library need to installed?
You can see this tutorial and cross-check with your method: View location data sent by NEO-M6 GPS using ESP32 board
The problem lies here: HardwareSerial GPS_serial(2);
The esp32c3 only has 2 uart’s: uart0 is usually mapped to the USB-CDC interface and uart1 is mapped to d6 & d7.
So changing to GPS_serial(1); should fix your problem.
Not quite correct. There are 3 “usable” serial ports on the ESP32-C3.