GPRS Shield (Seed)+ SD Shield (Seed)=> Transmit file by FTP

Hello

I try to send file from my sd card by ftp but no data are transmit, please HELP !!!

[code]#include <SoftwareSerial.h>
#include <String.h>
#include <SD.h>

File myFile;
SoftwareSerial mySerial(7, 8);

void setup()
{
mySerial.begin(19200);
Serial.begin(19200);

Serial.println(“Hello, INIT”);
delay(500);

//digitalWrite(9, HIGH);
//delay(1000);
//digitalWrite(9, LOW);
//Serial.println(“Sim900 ON”);
//delay(5000);

Serial.print(“Initializing SD card…”);
pinMode(10, OUTPUT);
if (!SD.begin(4)) {
Serial.println(“initialization SD failed!”);
return;
}
Serial.println(“initialization SD done.”);
Serial.println(“End of INIT”);

Serial.println(“ftp”);
myFile = SD.open(“test.txt”);

mySerial.println("AT+SAPBR=3,1,\"Contype\",\"GPRS\"");    //Configures GPRS connection
delay(100);
ShowSerialData();
mySerial.println("AT+SAPBR=3,1,\"APN\",\"FREE\"");
delay(100);
ShowSerialData();
mySerial.println("AT+SAPBR=1,1");
delay(100);
ShowSerialData();
mySerial.println("AT+FTPCID=1");    //Selects profile 1 for FTP operations
delay(1000);
ShowSerialData();
mySerial.println("AT+FTPSERV=\"ftp.xxxx.com\"");    //Configures FTP parameters
delay(2000);
ShowSerialData();
mySerial.println("AT+FTPPORT=21");
delay(2000);
ShowSerialData();
mySerial.println("AT+FTPUN=\"xxxx\"");
delay(2000);
ShowSerialData();
mySerial.println("AT+FTPPW=\"xxxxx\"");
delay(2000);
ShowSerialData();
mySerial.println("AT+FTPPUTNAME=\"test.txt\"");    //Sets destiny file name
delay(2000);
ShowSerialData();
mySerial.println("AT+FTPPUTPATH=\"/\"");    //Sets destiny file path
delay(2000);
ShowSerialData();
mySerial.println("AT+FTPPUT=1");    //Starts session
delay(2000); 
ShowSerialData();
mySerial.println("+FTPPUT:1,1,1200");
delay(2000); 
ShowSerialData();
mySerial.println("AT+FTPPUT=2,0");
delay(2000); 
ShowSerialData();
mySerial.println("+FTPPUT:1,0");
delay(2000); 
ShowSerialData();

}

void loop()
{

}

void ShowSerialData()
{
while(mySerial.available()!=0)
Serial.write(mySerial.read());
}[/code]

On my serveur I have the file but with 0 octet …

Answer on my serial:

[code]OK
AT+SAPBR=3,1,“APN”,“FREE”

OK
AT+SAPBR=1,1

+CME ERROR: 3
AT+FTPCID=1

OK
AT+FTPSERV=“ftp.xxxxx.com”

OK
AT+FTPPORT=21

OK
AT+FTPUN=“xxxx”

OK
AT+FTPPW=“xxxxx”

OK
AT+FTPPUTNAME=“test.txt”

OK
AT+FTPPUTPATH="/"

OK
AT+FTPPUT=1

OK
+FTPPUT:1,1,1200

+FTPPUT:1,1,1200
AT+FTPPUT=2,0

OK
+FTPPUT:1,0[/code]

Error “+CME ERROR: 3” may be the key problem, I sugest you to send “AT+CSTT”, “AT+CIICR”, “AT+CIFSR” before “AT+SAPBR=1,1”.

Have you found a solution to this? I’m also getting the new filename but no data sent over.