Getting Started with Wio Terminal

I have installed arduino and am trying to upload the blink example. All is well until the upload and I get the following error. I am using MacBook ok Pro Monterey.

Thanks

Arduino: 1.8.19 (Mac OS X), Board: “Seeeduino Wio Terminal, Master, Enabled, 120 MHz (standard), Small (-Os) (standard), 50 MHz (standard), Arduino, Off, On”

Sketch uses 31004 bytes (6%) of program storage space. Maximum is 507904 bytes.
java.io.IOException: Cannot run program “/Users/rich/Library/Arduino15/packages/Seeeduino/tools/bossac/1.8.0-48-gb176eee/bossac”: error=13, Permission denied
at java.lang.ProcessBuilder.start(ProcessBuilder.java:1048)
at java.lang.Runtime.exec(Runtime.java:620)
at java.lang.Runtime.exec(Runtime.java:485)
at processing.app.helpers.ProcessUtils.exec(ProcessUtils.java:11)
at cc.arduino.packages.Uploader.executeUploadCommand(Uploader.java:129)
at cc.arduino.packages.uploaders.SerialUploader.runCommand(SerialUploader.java:383)
at cc.arduino.packages.uploaders.SerialUploader.uploadUsingPreferences(SerialUploader.java:197)
at cc.arduino.UploaderUtils.upload(UploaderUtils.java:77)
at processing.app.SketchController.upload(SketchController.java:732)
at processing.app.SketchController.exportApplet(SketchController.java:703)
at processing.app.Editor$UploadHandler.run(Editor.java:2061)
at java.lang.Thread.run(Thread.java:748)
Caused by: java.io.IOException: error=13, Permission denied
at java.lang.UNIXProcess.forkAndExec(Native Method)
at java.lang.UNIXProcess.(UNIXProcess.java:247)
at java.lang.ProcessImpl.start(ProcessImpl.java:134)
at java.lang.ProcessBuilder.start(ProcessBuilder.java:1029)
… 11 more
An error occurred while uploading the sketch

This report would have more information with
“Show verbose output during compilation”
option enabled in File → Preferences.

I have the same error on Mac OS Monterey, installed on Intel Mac. Did you find any solution @richas?

Sorry, I did not. Let me know if you do. :wink:

Same problem here using mac, if someone find the solution , thanks for sharing

I found this solution :
run in the terminal
sudo chmod -R 755 /Users/<your_user>/Library/Arduino15/packages/Seeeduino/tools/bossac/1.8.0-48-gb176eee/bossac