Epididymitis, especially chronic epididymitis commonly occurs with chronic prostatitis and chronic seminal vesiculitis. During the inflammatory period, the tube of epididymis will become slim and even blocked. When two tubes are blocked, infertility happens.
Infection disease is a cause male infertility. Genital organs for men including genitals, accessory gland, epididymis and testicles can be infected by bacteria, chlamydia, mycoplasma, virus and other inflammation, leading inflammation to those organs.
Prostatitis, especially chronic prostatitis is a common disease for men. When this disease becomes severest, men can experience impotence, premature ejaculation and so on, thus, men’s reproductive ability can be affected greatly. It is easy for seminal vesiculitis turns into chronic type. This disease commonly occurs with chronic prostatitis and other chronic genital diseases, thus, it is easy to relapse.
Prostatitis, no matter is caused by virus or bacterial infection, can affect spermatogenic ability, especially when there are bacteria in semen, thus, men’s reproductive ability can be affected greatly.
Orchitis is complication of epididymitis. When orchitis becomes severe, it will develop into epididymo-orchitis. No matter inflammation is from testicles and other systems, it will hurt testicles. Testicles are factory of sperm, thus, if two testicles are damaged the reproductive ability is damaged.
Epididymitis and chronic prostatitis commonly occurs with chronic prostatitis and seminal vesiculitis. If this disease cannot be cured timely, inflammation can form scars and make it slim and even blocked it. Thus, if the two tubes are blocked, the reproductive ability is damaged.
Genital diseases can be cured by herbal medicine named Diuretic and Anti-inflammatory Pill. This herbal medicine has advantages such as promoting blood circulation, improving Qi, dissipating hard lumps; dissolving stasis and even releasing Pain. This herbal medicine also has advantages such as improving self-healing ability.