I have a brand new recomputer J1010 with a P-3448 B01 Jetson Nano module. I cannot get the board to boot after a flash with either Nvidia’s SDK Manager or manually at the command line. I have done this many times on my Jetson Orin AGX so am familiar with the process.
The flashing process, with either method, reports success. However, upon reboot the Nano hangs at the Nvidia Logo screen. I attached a UART to capture the output and I see that the output includes a reference to the 2GiB DRAM version, whereas this is the 4GiB. Below is the output from the UART:
[0000.203] [L4T TegraBoot] (version 00.00.2018.01-l4t-b1625959)
[0000.208] Processing in cold boot mode Bootloader 2
[0000.213] A02 Bootrom Patch rev = 1023
[0000.217] Power-up reason: software reset
[0000.220] No Battery Present
[0000.223] pmic max77620 reset reason
[0000.226] pmic max77620 NVERC : 0x0
[0000.230] RamCode = 1
[0000.232] Platform has DDR4 type RAM
[0000.235] max77620 disabling SD1 Remote Sense
[0000.239] Setting DDR voltage to 1125mv
[0000.243] Serial Number of Pmic Max77663: 0x24306a
[0000.251] Entering ramdump check
[0000.254] Get RamDumpCarveOut = 0x0
[0000.257] RamDumpCarveOut=0x0, RamDumperFlag=0xe59ff3f8
[0000.262] Last reboot was clean, booting normally!
[0000.267] Sdram initialization is successful
[0000.271] SecureOs Carveout Base=0x00000000ff800000 Size=0x00800000
[0000.277] Lp0 Carveout Base=0x00000000ff780000 Size=0x00001000
[0000.283] BpmpFw Carveout Base=0x00000000ff700000 Size=0x00080000
[0000.289] GSC1 Carveout Base=0x00000000ff600000 Size=0x00100000
[0000.295] GSC2 Carveout Base=0x00000000ff500000 Size=0x00100000
[0000.301] GSC4 Carveout Base=0x00000000ff400000 Size=0x00100000
[0000.306] GSC5 Carveout Base=0x00000000ff300000 Size=0x00100000
[0000.312] GSC3 Carveout Base=0x00000000bf300000 Size=0x00d00000
[0000.328] RamDump Carveout Base=0x00000000ff280000 Size=0x00080000
[0000.335] Platform-DebugCarveout: 0
[0000.338] Nck Carveout Base=0x00000000ff080000 Size=0x00200000
[0000.344] Non secure mode, and RB not enabled.
[0000.348] *** Booting BFS0.
[0000.350] NvTbootFailControlDoFailover: No failover; Continuing …
[0000.356] Read PT from (0:3)
[0000.371] Csd NumOfBlocks=0
[0000.410] PT crc32 and magic check passed.
[0000.414] Using BFS PT to query partitions
[0000.418] PT: Partition LNX NOT found !
[0000.422] *** Booting KFS0.
[0000.425] NvTbootFailControlDoFailover: No failover; Continuing …
[0000.431] BoardID = 3448, SKU = 0x2
[0000.434] Not Nano-SD or !QSPI-ONLY, check GPT table first …
[0000.439] Read GPT from (0:3)
[0000.448] Using GPT Primary to query partitions
[0000.453] NvTbootFailControlDoFailover: No failover; Continuing …
[0000.459] Loading Tboot-CPU binary
[0000.465] Verifying TBC in OdmNonSecureSBK mode
[0000.476] Bootloader load address is 0xa0000000, entry address is 0xa0000258
[0000.483] Bootloader downloaded successfully.
[0000.487] Downloaded Tboot-CPU binary to 0xa0000258
[0000.492] MAX77620_GPIO5 configured
[0000.495] CPU power rail is up
[0000.498] CPU clock enabled
[0000.502] Performing RAM repair
[0000.505] Updating A64 Warmreset Address to 0xa00002e9
[0000.510] BoardID = 3448, SKU = 0x2
[0000.513] Not Nano-SD or !QSPI-ONLY, check GPT table first …
[0000.519] NvTbootFailControlDoFailover: No failover; Continuing …
[0000.525] Loading NvTbootBootloaderDTB
[0000.542] Verifying NvTbootBootloaderDTB in OdmNonSecureSBK mode
[0000.614] Bootloader DTB Load Address: 0x83000000
[0000.618] BoardID = 3448, SKU = 0x2
[0000.622] Not Nano-SD or !QSPI-ONLY, check GPT table first …
[0000.627] Loading NvTbootKernelDTB
[0000.644] Verifying NvTbootKernelDTB in OdmNonSecureSBK mode
[0000.715] Kernel DTB Load Address: 0x83100000
[0000.719] BoardID = 3448, SKU = 0x2
[0000.723] Not Nano-SD or !QSPI-ONLY, check GPT table first …
[0000.729] NvTbootFailControlDoFailover: No failover; Continuing …
[0000.736] Loading cboot binary
[0000.747] Verifying EBT in OdmNonSecureSBK mode
[0000.789] Bootloader load address is 0x92c00000, entry address is 0x92c00258
[0000.796] Bootloader downloaded successfully.
[0000.800] BoardID = 3448, SKU = 0x2
[0000.803] Not Nano-SD or !QSPI-ONLY, check GPT table first …
[0000.809] NvTbootFailControlDoFailover: No failover; Continuing …
[0000.815] PT: Partition NCT NOT found !
[0000.819] Warning: Find Partition via PT Failed
[0000.823] Next binary entry address: 0x92c00258
[0000.828] BoardId: 3448
[0000.832] Overriding pmu board id with proc board id
[0000.837] Display board id is not available
[0000.841] BoardID = 3448, SKU = 0x2
[0000.845] Not Nano-SD or !QSPI-ONLY, check GPT table first …
[0000.851] NvTbootFailControlDoFailover: No failover; Continuing …
[0000.864] Verifying SC7EntryFw in OdmNonSecureSBK mode
[0000.954] /bpmp deleted
[0000.956] SC7EntryFw header found loaded at 0xff700000
[0001.364] OVR2 PMIC
[0001.366] Bpmp FW successfully loaded
[0001.369] BoardID = 3448, SKU = 0x2
[0001.372] Not Nano-SD or !QSPI-ONLY, check GPT table first …
[0001.378] NvTbootFailControlDoFailover: No failover; Continuing …
[0001.386] WB0 init successfully at 0xff780000
[0001.390] Verifying NvTbootWb0 in OdmNonSecureSBK mode
[0001.395] Set NvDecSticky Bits
[0001.399] GSC2 address ff53fffc value c0edbbcc
[0001.405] GSC MC Settings done
[0001.408] BoardID = 3448, SKU = 0x2
[0001.411] Not Nano-SD or !QSPI-ONLY, check GPT table first …
[0001.418] TOS Image length 53680
[0001.421] Monitor size 53680
[0001.423] OS size 0
[0001.429] Secure Os AES-CMAC Verification Success!
[0001.434] TOS image cipher info: plaintext
[0001.437] Loading and Validation of Secure OS Successful
[0001.453] SC7 Entry Firmware - 0xff700000, 0x4000
[0001.458] NvTbootPackSdramParams: start.
[0001.463] NvTbootPackSdramParams: done.
[0001.467] Tegraboot started after 131941 us
[0001.471] Basic modules init took 745921 us
[0001.475] Sec Bootdevice Read Time = 54 ms, Read Size = 3682 KB
[0001.481] Sec Bootdevice Write Time = 0 ms, Write Size = 0 KB
[0001.486] Next stage binary read took 7383 us
[0001.490] Carveout took -34774 us
[0001.493] CPU initialization took 651996 us
[0001.497] Total time taken by TegraBoot 1370526 us
[0001.502] Starting CPU & Halting co-processor
64NOTICE: BL31: v1.3(release):269577911
NOTICE: BL31: Built : 23:37:38, Nov 4 2024
ERROR: Error initializing runtime service trusty_fast
[0001.624] RamCode = 1
[0001.626] get_emc_table_offset: Can’t find emc-table node
[0001.631] LPDDR4 Training: Can’t find emc-table node
[0001.679]
[0001.680] Debug Init done
[0001.683] Marked DTB cacheable
[0001.686] Bootloader DTB loaded at 0x83000000
[0001.690] Marked DTB cacheable
[0001.693] Kernel DTB loaded at 0x83100000
[0001.697] DeviceTree Init done
[0001.712] Pinmux applied successfully
[0001.717] gicd_base: 0x50041000
[0001.720] gicc_base: 0x50042000
[0001.723] Interrupts Init done
[0001.728] Using base:0x60005090 & irq:208 for tick-timer
[0001.733] Using base:0x60005098 for delay-timer
[0001.737] platform_init_timer: DONE
[0001.741] Timer(tick) Init done
[0001.745] osc freq = 38400 khz
[0001.749]
[0001.750] Welcome to L4T Cboot
[0001.753]
[0001.754] Cboot Version: 00.00.2018.01-t210-acb23272
[0001.759] calling constructors
[0001.762] initializing heap
[0001.765] initializing threads
[0001.768] initializing timers
[0001.771] creating bootstrap completion thread
[0001.775] top of bootstrap2()
[0001.778] CPU: ARM Cortex A57
[0001.781] CPU: MIDR: 0x411FD071, MPIDR: 0x80000000
[0001.785] initializing platform
[0001.840] Config for emmc ddr50 mode completed
[0001.844] sdmmc bdev is already initialized
[0001.849] Enable APE clock
[0001.851] Un-powergate APE partition
[0001.855] of_register: registering tegra_udc to of_hal
[0001.860] of_register: registering inv20628-driver to of_hal
[0001.865] of_register: registering ads1015-driver to of_hal
[0001.871] of_register: registering lp8557-bl-driver to of_hal
[0001.877] of_register: registering bq2419x_charger to of_hal
[0001.882] of_register: registering bq27441_fuel_gauge to of_hal
[0001.895] gpio framework initialized
[0001.899] of_register: registering tca9539_gpio to of_hal
[0001.904] of_register: registering tca9539_gpio to of_hal
[0001.909] of_register: registering i2c_bus_driver to of_hal
[0001.915] of_register: registering i2c_bus_driver to of_hal
[0001.920] of_register: registering i2c_bus_driver to of_hal
[0001.926] pmic framework initialized
[0001.929] of_register: registering max77620_pmic to of_hal
[0001.935] regulator framework initialized
[0001.939] of_register: registering tps65132_bl_driver to of_hal
[0001.945] initializing target
[0001.951] gpio_driver_register: register ‘tegra_gpio_driver’ driver
[0001.960] board ID = D78, board SKU = 2
[0001.967] fixed regulator driver initialized
[0001.988] initializing OF layer
[0001.991] NCK carveout not present
[0001.994] Skipping dts_overrides
[0001.998] of_children_init: Ops found for compatible string nvidia,tegra210-i2c
[0002.017] I2C Bus Init done
[0002.020] of_children_init: Ops found for compatible string nvidia,tegra210-i2c
[0002.031] I2C Bus Init done
[0002.034] of_children_init: Ops found for compatible string nvidia,tegra210-i2c
[0002.045] I2C Bus Init done
[0002.047] of_children_init: Ops found for compatible string nvidia,tegra210-i2c
[0002.058] I2C Bus Init done
[0002.061] of_children_init: Ops found for compatible string nvidia,tegra210-i2c
[0002.072] I2C Bus Init done
[0002.075] of_children_init: Ops found for compatible string maxim,max77620
[0002.086] max77620_init using irq 118
[0002.091] register ‘maxim,max77620’ pmic
[0002.095] gpio_driver_register: register ‘max77620-gpio’ driver
[0002.101] of_children_init: Ops found for compatible string nvidia,tegra210-i2c
[0002.113] I2C Bus Init done
[0002.116] NCK carveout not present
[0002.128] Find /i2c@7000c000’s alias i2c0
[0002.131] get eeprom at 1-a0, size 256, type 0
[0002.141] Find /i2c@7000c500’s alias i2c2
[0002.145] get eeprom at 3-a0, size 256, type 0
[0002.150] get eeprom at 3-ae, size 256, type 0
[0002.154] pm_ids_update: Updating 1,a0, size 256, type 0
[0002.159] I2C slave not started
[0002.162] I2C write failed
[0002.165] Writing offset failed
[0002.168] eeprom_init: EEPROM read failed
[0002.172] pm_ids_update: eeprom init failed
[0002.176] pm_ids_update: Updating 3,a0, size 256, type 0
[0002.206] pm_ids_update: The pm board id is 3448-0002-402
[0002.213] Adding plugin-manager/ids/3448-0002-402=/i2c@7000c500:module@0x50
[0002.222] pm_ids_update: pm id update successful
[0002.226] pm_ids_update: Updating 3,ae, size 256, type 0
[0002.256] pm_ids_update: The pm board id is 3449-0000-rXj
[0002.263] Adding plugin-manager/ids/3449-0000-rXj=/i2c@7000c500:module@0x57
[0002.271] pm_ids_update: pm id update successful
[0002.302] eeprom_get_mac: EEPROM invalid MAC address (all 0xff)
[0002.307] shim_eeprom_update_mac:267: Failed to update 0 MAC address in DTB
[0002.316] eeprom_get_mac: EEPROM invalid MAC address (all 0xff)
[0002.321] shim_eeprom_update_mac:267: Failed to update 1 MAC address in DTB
[0002.330] updating /chosen/nvidia,ethernet-mac node 3c:6d:66:14:fb:35
[0002.336] Plugin Manager: Parse ODM data 0x000a4000
[0002.349] shim_cmdline_install: /chosen/bootargs: earlycon=uart8250,mmio32,0x70006000
[0002.366] Find /i2c@7000c000’s alias i2c0
[0002.369] get eeprom at 1-a0, size 256, type 0
[0002.379] Find /i2c@7000c500’s alias i2c2
[0002.383] get eeprom at 3-a0, size 256, type 0
[0002.388] get eeprom at 3-ae, size 256, type 0
[0002.392] pm_ids_update: Updating 1,a0, size 256, type 0
[0002.397] I2C slave not started
[0002.400] I2C write failed
[0002.403] Writing offset failed
[0002.406] eeprom_init: EEPROM read failed
[0002.410] pm_ids_update: eeprom init failed
[0002.414] pm_ids_update: Updating 3,a0, size 256, type 0
[0002.444] pm_ids_update: The pm board id is 3448-0002-402
[0002.451] Adding plugin-manager/ids/3448-0002-402=/i2c@7000c500:module@0x50
[0002.458] pm_ids_update: pm id update successful
[0002.462] pm_ids_update: Updating 3,ae, size 256, type 0
[0002.492] pm_ids_update: The pm board id is 3449-0000-rXj
[0002.499] Adding plugin-manager/ids/3449-0000-rXj=/i2c@7000c500:module@0x57
[0002.506] pm_ids_update: pm id update successful
[0002.536] Add serial number:1424624336376 as DT property
[0002.544] Applying platform configs
[0002.552] platform-init is not present. Skipping
[0002.556] calling apps_init()
[0002.577] Found 17 GPT partitions in “sdmmc3_user”
[0002.582] Proceeding to Cold Boot
[0002.585] starting app android_boot_app
[0002.589] Device state: unlocked
[0002.592] display console init
[0002.602] could not find regulator
[0002.625] hdmi cable not connected
[0002.629] is_hdmi_neeDT entry for leds-pwm not found
d[0002.638] ed: HDMI not connected, returning false
[0002.642] hdmi is not connected
[0002.645] sor0 is not supported
[0002.648] display_console_init: no valid display out_type
[0002.657] subnode volume_up is not found !
[0002.661] subnode back is not found !
[0002.664] subnode volume_down is not found !
[0002.669] subnode menu is not found !
[0002.672] Gpio keyboard init success
[0002.720] found decompressor handler: lz4-legacy
[0002.734] decompressing blob (type 1)…
[0002.799] display_resolution: No display init
[0002.803] Failed to retrieve display resolution
[0002.807] Could not load/initialize BMP blob…ignoring
[0002.813] -------> se_aes_verify_sbk_clear: 747
[0002.817] se_aes_verify_sbk_clear: Error
[0002.821] SE operation failed
[0002.824] bl_battery_charging: connected to external power supply
[0002.834] display_console_ioctl: No display init
[0002.838] switch_backlight failed
[0002.848] device_query_partition_size: failed to open partition sdmmc3_user:MSC !
[0002.855] MSC Partition not found
[0002.865] device_query_partition_size: failed to open partition sdmmc3_user:USP !
[0002.872] USP partition read failed!
[0002.876] blob_init: blob-partition USP header read failed
[0002.881] android_boot Unable to update recovery partition
[0002.887] kfs_getpartname: name = LNX
[0002.890] Loading kernel from LNX
[0002.983] load kernel from storage
[0002.993] decompressor handler not found
[0003.027] Successfully loaded kernel and ramdisk images
[0003.032] board ID = D78, board SKU = 2
[0003.037] display_resolution: No display init
[0003.041] Failed to retrieve display resolution
[0003.045] bmp blob is not loaded and initialized
[0003.050] Failed to display boot-logo
[0003.054] NCK carveout not present
[0003.057] Skipping dts_overrides
[0003.060] NCK carveout not present
[0003.071] Find /i2c@7000c000’s alias i2c0
[0003.075] get eeprom at 1-a0, size 256, type 0
[0003.085] Find /i2c@7000c500’s alias i2c2
[0003.089] get eeprom at 3-a0, size 256, type 0
[0003.093] get eeprom at 3-ae, size 256, type 0
[0003.098] pm_ids_update: Updating 1,a0, size 256, type 0
[0003.103] I2C slave not started
[0003.106] I2C write failed
[0003.109] Writing offset failed
[0003.112] eeprom_init: EEPROM read failed
[0003.116] pm_ids_update: eeprom init failed
[0003.120] pm_ids_update: Updating 3,a0, size 256, type 0
[0003.150] pm_ids_update: The pm board id is 3448-0002-402
[0003.157] Adding plugin-manager/ids/3448-0002-402=/i2c@7000c500:module@0x50
[0003.165] pm_ids_update: pm id update successful
[0003.170] pm_ids_update: Updating 3,ae, size 256, type 0
[0003.200] pm_ids_update: The pm board id is 3449-0000-rXj
[0003.207] Adding plugin-manager/ids/3449-0000-rXj=/i2c@7000c500:module@0x57
[0003.215] pm_ids_update: pm id update successful
[0003.245] eeprom_get_mac: EEPROM invalid MAC address (all 0xff)
[0003.251] shim_eeprom_update_mac:267: Failed to update 0 MAC address in DTB
[0003.259] eeprom_get_mac: EEPROM invalid MAC address (all 0xff)
[0003.265] shim_eeprom_update_mac:267: Failed to update 1 MAC address in DTB
[0003.274] updating /chosen/nvidia,ethernet-mac node 3c:6d:66:14:fb:35
[0003.280] Plugin Manager: Parse ODM data 0x000a4000
[0003.293] shim_cmdline_install: /chosen/bootargs: earlycon=uart8250,mmio32,0x70006000
[0003.301] Add serial number:1424624336376 as DT property
[0003.311] “bpmp” doesn’t exist, creating
[0003.317] Updated bpmp info to DTB
[0003.322] Updated initrd info to DTB
[0003.325] “proc-board” doesn’t exist, creating
[0003.332] Updated board info to DTB
[0003.335] “pmu-board” doesn’t exist, creating
[0003.341] Updated board info to DTB
[0003.344] “display-board” doesn’t exist, creating
[0003.350] Updated board info to DTB
[0003.354] “reset” doesn’t exist, creating
[0003.358] Updated reset info to DTB
[0003.362] display_console_ioctl: No display init
[0003.366] display_console_ioctl: No display init
[0003.371] display_console_ioctl: No display init
[0003.375] Cmdline: tegraid=21.1.2.0.0 ddr_die=2048M@2048M section=256M memtype=0 vpr_resize usb_port_owner_info=0 l
[0003.410] DTB cmdline: earlycon=uart8250,mmio32,0x70006000
[0003.415] boot image cmdline: root=/dev/mmcblk0p1 rw rootwait rootfstype=ext4 console=ttyS0,115200n8 console=tty0 f
[0003.432] Updated bootarg info to DTB
[0003.436] Adding uuid 000000016440b7400c00000012000140 to DT
[0003.441] Adding eks info 0 to DT
[0003.447] WARNING: Failed to pass NS DRAM ranges to TOS, err: -7
[0003.453] Updated memory info to DTB
[0003.462] set vdd_core voltage to 1125 mv
[0003.466] setting ‘vdd-core’ regulator to 1125000 micro volts
[0003.472] Found secure-pmc; disable BPMP
U-Boot 2020.04-g904285e3a7 (Nov 04 2024 - 23:37:42 -0800)
SoC: tegra210
Model: NVIDIA Jetson Nano Developer Kit
Board: NVIDIA P3450-0000
DRAM: 2 GiB
MMC: sdhci@700b0000: 1, sdhci@700b0600: 0
Loading Environment from MMC… *** Warning - bad CRC, using default environment
In: serial
Out: serial
Err: serial
Net: No ethernet found.
Hit any key to stop autoboot: 0
MMC: no card present
switch to partitions #0, OK
mmc0(part 0) is current device
Scanning mmc 0:1…
Found /boot/extlinux/extlinux.conf
Retrieving file: /boot/extlinux/extlinux.conf
879 bytes read in 22 ms (38.1 KiB/s)
1: primary kernel
Retrieving file: /boot/initrd
7160200 bytes read in 183 ms (37.3 MiB/s)
Retrieving file: /boot/Image
34707464 bytes read in 786 ms (42.1 MiB/s)
append: tegraid=21.1.2.0.0 ddr_die=2048M@2048M section=256M memtype=0 vpr_resize usb_port_owner_info=0 lane_owner_in
Flattened Device Tree blob at 83100000
Booting using the fdt blob at 0x83100000
ERROR: reserving fdt memory region failed (addr=0 size=0)
ERROR: reserving fdt memory region failed (addr=0 size=0)
Using Device Tree in place at 0000000083100000, end 000000008317ce8d
copying carveout for /host1x@50000000/dc@54200000…
copying carveout for /host1x@50000000/dc@54240000…
Starting kernel …
[ 0.000000] Booting Linux on physical CPU 0x0
[ 0.000000] Linux version 4.9.337-tegra (buildbrain@mobile-u64-5499-d7000) (gcc version 7.3.1 20180425 [linaro-7.4
[ 0.000000] Boot CPU: AArch64 Processor [411fd071]
[ 0.000000] OF: fdt:memory scan node memory@80000000, reg size 32,
[ 0.000000] OF: fdt: - 80000000 , 3f200000
[ 0.000000] OF: fdt: - c0000000 , 3ee00000
[ 0.000000] earlycon: uart8250 at MMIO32 0x0000000070006000 (options ‘’)
[ 0.000000] bootconsole [uart8250] enabled
I am wondering if the proper .dtb file is being applied. The Jetpack i’m flashing is 4.6.1 in the case of SDK Manager and Jetson Linux R32.7.6 in the CLI case. Note this section of the output which seems to indicate a different board:
SoC: tegra210
Model: NVIDIA Jetson Nano Developer Kit
Board: NVIDIA P3450-0000
DRAM: 2 GiB
Any help is greatly appreciated.