I am using a carrier board A206 from Seeed studio on which is mounted a nvme M.2 ssd.
Previously, I flashed my ssd with L4T 32.6.1 which worked perfectly fine.
I am now trying to flash the ssd with L4T 32.7.1. While the flashing appears to have been successful, I’m not getting any oem-config screen afterwards (no hdmi output).
I’ve been running a Jetson Xavier NX on the A206 with an nvme ssd using JetPack 4.6.1 (installed via sdkmanager), which uses L4T 32.7.1.
I’ve just upgraded to L4T 32.7.2 via sudo apt upgrade, but it required modifying the spec in /etc/nv_boot_control.conf with