Hi,
I am currently trying to flash a Jetson Orin NX 16GB with a J401 custom carrier board from Seeed studio on an Ubuntu 20.04 machine. I tried multiple methods for this:
- Following the flashing instructions from the official Seeed Studio J401 website. Tried different Jetpacks (5.1.1, 5.1.2 as well as 6).
- Following the SDK Manager method from NVIDIA.
The flashing process always ends up in failure at the tar: Read Checkpoint xxxxx stage with different checkpoint every time. I have tried flashing with different versions of Ubuntu (24.04, 22.04 and 20.04) with same result which tells me the problem does not lie with the OS. I have also used different USB-C cables for flashing which also did not give a different result.
I came across this post and tried the solution of formatting the SSD with a single ext4 partition but that did not help either. I am using a Samsung 980 Pro 2TB SSD (in case that is of relevance).
The logs attached with the post are with trying to flash with Jetpack 5.1.1
If someone has an idea about how I can proceed here, it would be greatly appreciated.
Thank you!
/home/itk/jetson_orin_flashing/downloaded/mfi_recomputer-orin-j401/recomputer-orin-j401.conf: line 29: /home/itk/jetson_orin_flashing/downloaded/mfi_recomputer-orin-j401/p3768-0000-p3767-0000-a0.conf: No such file or directory
/home/itk/jetson_orin_flashing/downloaded/mfi_recomputer-orin-j401/recomputer-orin-j401.conf: line 29: /home/itk/jetson_orin_flashing/downloaded/mfi_recomputer-orin-j401/p3768-0000-p3767-0000-a0.conf: No such file or directory
/home/itk/jetson_orin_flashing/downloaded/mfi_recomputer-orin-j401/tools/kernel_flash/l4t_initrd_flash_internal.sh --network usb0 --usb-instance 3-2 --device-instance 0 --flash-only --external-device nvme0n1p1 -c "tools/kernel_flash/flash_l4t_nvme.xml" -S 80GiB --network usb0 recomputer-orin-j401 external
/home/itk/jetson_orin_flashing/downloaded/mfi_recomputer-orin-j401/recomputer-orin-j401.conf: line 29: /home/itk/jetson_orin_flashing/downloaded/mfi_recomputer-orin-j401/p3768-0000-p3767-0000-a0.conf: No such file or directory
# Entry added by NVIDIA initrd flash tool
/home/itk/jetson_orin_flashing/downloaded/mfi_recomputer-orin-j401/tools/kernel_flash/tmp 127.0.0.1(rw,nohide,insecure,no_subtree_check,async,no_root_squash)
Export list for localhost:
/home/itk/jetson_orin_flashing/downloaded/mfi_recomputer-orin-j401/tools/kernel_flash/tmp 127.0.0.1
/home/itk/jetson_orin_flashing/downloaded/mfi_recomputer-orin-j401/recomputer-orin-j401.conf: line 29: /home/itk/jetson_orin_flashing/downloaded/mfi_recomputer-orin-j401/p3768-0000-p3767-0000-a0.conf: No such file or directory
**********************************************
* *
* Step 1: Build the flashing environment *
* *
**********************************************
Create flash environment 0
/home/itk/jetson_orin_flashing/downloaded/mfi_recomputer-orin-j401/bootloader /home/itk/jetson_orin_flashing/downloaded/mfi_recomputer-orin-j401
/home/itk/jetson_orin_flashing/downloaded/mfi_recomputer-orin-j401
Finish creating flash environment 0.
****************************************************
* *
* Step 2: Boot the device with flash initrd image *
* *
****************************************************
/home/itk/jetson_orin_flashing/downloaded/mfi_recomputer-orin-j401/temp_initrdflash/bootloader0 /home/itk/jetson_orin_flashing/downloaded/mfi_recomputer-orin-j401
./tegraflash.py --bl uefi_jetson_with_dtb_sigheader.bin.encrypt --bct br_bct_BR.bct --securedev --bldtb tegra234-j401-p3768-0000+p3767-0000-recomputer.dtb --applet rcm_2_encrypt.rcm --applet_softfuse rcm_1_encrypt.rcm --cmd "rcmboot" --cfg secureflash.xml --chip 0x23 --mb1_bct mb1_bct_MB1_sigheader.bct.encrypt --mem_bct mem_rcm_sigheader.bct.encrypt --mb1_cold_boot_bct mb1_cold_boot_bct_MB1_sigheader.bct.encrypt --mb1_bin mb1_t234_prod_aligned_sigheader.bin.encrypt --psc_bl1_bin psc_bl1_t234_prod_aligned_sigheader.bin.encrypt --mem_bct_cold_boot mem_coldboot_sigheader.bct.encrypt --bins "psc_fw pscfw_t234_prod_sigheader.bin.encrypt; mts_mce mce_flash_o10_cr_prod_sigheader.bin.encrypt; tsec_fw tsec_t234_sigheader.bin.encrypt; mb2_applet applet_t234_sigheader.bin.encrypt; mb2_bootloader mb2_t234_with_mb2_cold_boot_bct_MB2_sigheader.bin.encrypt; xusb_fw xusb_t234_prod_sigheader.bin.encrypt; pva_fw nvpva_020_sigheader.fw.encrypt; dce_fw display-t234-dce_sigheader.bin.encrypt; nvdec nvdec_t234_prod_sigheader.fw.encrypt; bpmp_fw bpmp_t234-TE980M-A1_prod_sigheader.bin.encrypt; bpmp_fw_dtb tegra234-bpmp-3767-0000-a02-3509-a02_with_odm_sigheader.dtb.encrypt; rce_fw camera-rtcpu-t234-rce_sigheader.img.encrypt; ape_fw adsp-fw_sigheader.bin.encrypt; spe_fw spe_t234_sigheader.bin.encrypt; tos tos-optee_t234_sigheader.img.encrypt; eks eks_t234_sigheader.img.encrypt; kernel boot0.img; kernel_dtb tegra234-j401-p3768-0000+p3767-0000-recomputer.dtb" --bct_backup --instance 3-2
/home/itk/jetson_orin_flashing/downloaded/mfi_recomputer-orin-j401/temp_initrdflash/bootloader0/tegraflash_internal.py:1272: SyntaxWarning: invalid escape sequence '\.'
patt = re.compile(".*(mbr|gpt).*\.bin")
/home/itk/jetson_orin_flashing/downloaded/mfi_recomputer-orin-j401/temp_initrdflash/bootloader0/tegraflash_internal.py:1388: SyntaxWarning: invalid escape sequence '\.'
patt = re.compile(".*(mbr|gpt).*\.bin")
/home/itk/jetson_orin_flashing/downloaded/mfi_recomputer-orin-j401/temp_initrdflash/bootloader0/tegraflash_internal.py:4587: SyntaxWarning: invalid escape sequence '\s'
m = re.search('bpmp_fw_dtb[\s]+([\w._-]+)', values['--bins'])
/home/itk/jetson_orin_flashing/downloaded/mfi_recomputer-orin-j401/temp_initrdflash/bootloader0/tegrasign_v3_internal.py:1124: SyntaxWarning: invalid escape sequence '\d'
m = re.search('Key size is (\d+)', ret_str)
/home/itk/jetson_orin_flashing/downloaded/mfi_recomputer-orin-j401/temp_initrdflash/bootloader0/tegrasign_v3_internal.py:1169: SyntaxWarning: invalid escape sequence '\d'
m = re.search('Key size is (\d+)', ret_str)
/home/itk/jetson_orin_flashing/downloaded/mfi_recomputer-orin-j401/temp_initrdflash/bootloader0/tegrasign_v3_internal.py:1527: SyntaxWarning: invalid escape sequence '\d'
re_string = 'kdf_args_' + temp_stem + '(\d).yaml'
/home/itk/jetson_orin_flashing/downloaded/mfi_recomputer-orin-j401/temp_initrdflash/bootloader0/tegraflash_impl_t234.py:1480: SyntaxWarning: invalid escape sequence '\s'
m = re.search('bpmp_fw_dtb[\s]+([\w._-]+)', values['--bins'])
/home/itk/jetson_orin_flashing/downloaded/mfi_recomputer-orin-j401/temp_initrdflash/bootloader0/tegraflash_impl_t234.py:2942: SyntaxWarning: invalid escape sequence '\.'
patt = re.compile(".*(mbr|gpt).*\.bin")
/home/itk/jetson_orin_flashing/downloaded/mfi_recomputer-orin-j401/temp_initrdflash/bootloader0/tegraflash_impl_t234.py:3004: SyntaxWarning: invalid escape sequence '\/'
info_print("Copying enc\/signed file in " + output_dir)
Welcome to Tegra Flash
version 1.0.0
Type ? or help for help and q or quit to exit
Use ! to execute system commands
Entering RCM boot
[ 0.0293 ] mb1_t234_prod_aligned_sigheader.bin.encrypt filename is from --mb1_bin
[ 0.0293 ] psc_bl1_t234_prod_aligned_sigheader.bin.encrypt filename is from --psc_bl1_bin
[ 0.0293 ] rcm boot with presigned binaries
[ 0.0298 ] tegrarcm_v2 --instance 3-2 --new_session --chip 0x23 0 --uid --download bct_br br_bct_BR.bct --download mb1 mb1_t234_prod_aligned_sigheader.bin.encrypt --download psc_bl1 psc_bl1_t234_prod_aligned_sigheader.bin.encrypt --download bct_mb1 mb1_bct_MB1_sigheader.bct.encrypt
[ 0.0301 ] BR_CID: 0x80012344705DE522400000000EFD80C0
[ 0.0393 ] Sending bct_br
[ 0.0464 ] Sending mb1
[ 0.0469 ] Sending psc_bl1
[ 0.0567 ] Sending bct_mb1
[ 0.0625 ] Generating blob for T23x
[ 0.0640 ] tegrahost_v2 --chip 0x23 0 --generateblob blob.xml blob.bin
[ 0.0642 ] The number of images in blob is 19
[ 0.0646 ] blobsize is 107839651
[ 0.0647 ] Added binary blob_uefi_jetson_with_dtb_sigheader.bin.encrypt of size 3592256
[ 0.0993 ] Added binary blob_pscfw_t234_prod_sigheader.bin.encrypt of size 310768
[ 0.1001 ] Added binary blob_mce_flash_o10_cr_prod_sigheader.bin.encrypt of size 187120
[ 0.1004 ] Added binary blob_tsec_t234_sigheader.bin.encrypt of size 176128
[ 0.1006 ] Added binary blob_applet_t234_sigheader.bin.encrypt of size 279616
[ 0.1008 ] Not supported type: mb2_applet
[ 0.1009 ] Added binary blob_mb2_t234_with_mb2_cold_boot_bct_MB2_sigheader.bin.encrypt of size 439968
[ 0.1012 ] Added binary blob_xusb_t234_prod_sigheader.bin.encrypt of size 164864
[ 0.1014 ] Added binary blob_nvpva_020_sigheader.fw.encrypt of size 2164640
[ 0.1019 ] Added binary blob_display-t234-dce_sigheader.bin.encrypt of size 12065552
[ 0.1091 ] Added binary blob_nvdec_t234_prod_sigheader.fw.encrypt of size 294912
[ 0.1114 ] Added binary blob_bpmp_t234-TE980M-A1_prod_sigheader.bin.encrypt of size 1027008
[ 0.1119 ] Added binary blob_tegra234-bpmp-3767-0000-a02-3509-a02_with_odm_sigheader.dtb.encrypt of size 383232
[ 0.1121 ] Added binary blob_camera-rtcpu-t234-rce_sigheader.img.encrypt of size 458096
[ 0.1123 ] Added binary blob_adsp-fw_sigheader.bin.encrypt of size 414976
[ 0.1124 ] Added binary blob_spe_t234_sigheader.bin.encrypt of size 270336
[ 0.1125 ] Added binary blob_tos-optee_t234_sigheader.img.encrypt of size 1633344
[ 0.1131 ] Added binary blob_eks_t234_sigheader.img.encrypt of size 9232
[ 0.1133 ] Added binary blob_boot0.img of size 83722240
[ 0.1498 ] Added binary blob_tegra234-j401-p3768-0000+p3767-0000-recomputer.dtb of size 244259
[ 0.2001 ] tegrarcm_v2 --instance 3-2 --chip 0x23 0 --pollbl --download bct_mem mem_rcm_sigheader.bct.encrypt --download blob blob.bin
[ 0.2002 ] BL: version 1.4.0.2-t234-54845784-08a4de08 last_boot_error: 0
[ 0.3239 ] Sending bct_mem
[ 0.3312 ] Sending blob
[ 3.9744 ] RCM-boot started
/home/itk/jetson_orin_flashing/downloaded/mfi_recomputer-orin-j401
***************************************
* *
* Step 3: Start the flashing process *
* *
***************************************
chown: warning: '.' should be ':': ‘root.root’
chown: warning: '.' should be ':': ‘root.root’
Waiting for target to boot-up...
Waiting for target to boot-up...
Waiting for target to boot-up...
Waiting for target to boot-up...
Waiting for target to boot-up...
Waiting for target to boot-up...
Waiting for target to boot-up...
Waiting for target to boot-up...
Waiting for target to boot-up...
Waiting for target to boot-up...
Waiting for target to boot-up...
Waiting for target to boot-up...
Waiting for target to boot-up...
Waiting for target to boot-up...
Waiting for target to boot-up...
Waiting for target to boot-up...
Waiting for target to boot-up...
Waiting for target to boot-up...
Waiting for target to boot-up...
Waiting for target to boot-up...
Waiting for target to boot-up...
Waiting for target to boot-up...
Waiting for device to expose ssh ......Waiting for device to expose ssh ...Run command: flash on fc00:1:1:0::2
SSH ready
blockdev: cannot open /dev/mmcblk0boot0: No such file or directory
[ 0]: l4t_flash_from_kernel: Serial Number: 1424223006194
[ 0]: l4t_flash_from_kernel: Starting to create gpt for emmc
Active index file is /mnt/internal/flash.idx
Number of lines is 61
max_index=60
[ 1]: l4t_flash_from_kernel: Successfully create gpt for emmc
[ 1]: l4t_flash_from_kernel: Starting to create gpt for external device
Active index file is /mnt/external/flash.idx
Number of lines is 18
max_index=17
writing item=1, 9:0:primary_gpt, 512, 19968, gpt_primary_9_0.bin, 16896, fixed-<reserved>-0, 577cc6c87532c9c1214871dc0ca89531d7af1972
Writing primary_gpt partition with gpt_primary_9_0.bin
Offset is not aligned to K Bytes, no optimization is applied
dd if=/mnt/external/gpt_primary_9_0.bin of=/dev/nvme0n1 bs=1 skip=0 seek=512 count=16896
16896+0 records in
16896+0 records out
16896 bytes (17 kB, 16 KiB) copied, 0.0221494 s, 763 kB/s
Writing primary_gpt partition done
Error: The backup GPT table is corrupt, but the primary appears OK, so that will be used.
Warning: Not all of the space available to /dev/nvme0n1 appears to be used, you can fix the GPT to use all of the space (an extra 3707029168 blocks) or continue with the current setting?
Writing secondary_gpt partition with gpt_secondary_9_0.bin
Offset is not aligned to K Bytes, no optimization is applied
dd if=/mnt/external/gpt_secondary_9_0.bin of=/dev/nvme0n1 bs=1 skip=0 seek=102399983104 count=16896
16896+0 records in
16896+0 records out
16896 bytes (17 kB, 16 KiB) copied, 0.0231018 s, 731 kB/s
Writing secondary_gpt partition done
Fix/Ignore? Warning: Not all of the space available to /dev/nvme0n1 appears to be used, you can fix the GPT to use all of the space (an extra 3707029168 blocks) or continue with the current setting?
Fix
Model: Samsung SSD 980 PRO 2TB (nvme)
Disk /dev/nvme0n1: 2000GB
Sector size (logical/physical): 512B/512B
Partition Table: gpt
Disk Flags:
Number Start End Size File system Name Flags
2 20.5kB 134MB 134MB A_kernel msftdata
3 134MB 135MB 786kB A_kernel-dtb msftdata
4 135MB 168MB 33.2MB A_reserved_on_user msftdata
5 168MB 302MB 134MB B_kernel msftdata
6 302MB 303MB 786kB B_kernel-dtb msftdata
7 303MB 336MB 33.2MB B_reserved_on_user msftdata
8 336MB 420MB 83.9MB recovery msftdata
9 420MB 421MB 524kB recovery-dtb msftdata
10 421MB 488MB 67.1MB fat32 esp boot, esp
11 488MB 572MB 83.9MB recovery_alt msftdata
12 572MB 572MB 524kB recovery-dtb_alt msftdata
13 572MB 639MB 67.1MB esp_alt msftdata
14 639MB 1059MB 419MB UDA msftdata
15 1059MB 1562MB 503MB reserved msftdata
1 1562MB 102GB 101GB ext4 APP msftdata
[ 16]: l4t_flash_from_kernel: Expanding last partition to fill the storage device
[ 16]: l4t_flash_from_kernel: Successfully create gpt for external device
[ 16]: l4t_flash_from_kernel: Starting to flash to external device
[ 16]: l4t_flash_from_kernel: Starting to flash to emmc
Active index file is /mnt/external/flash.idx
Active index file is /mnt/internal/flash.idx
Flash index file is /mnt/internal/flash.idx
Number of lines is 61
max_index=60
Number of lines is 18
max_index=17
Number of lines is 61
max_index=60
[ 16]: l4t_flash_from_kernel: Starting to flash to qspi
writing item=0, 9:0:master_boot_record, 0, 512, mbr_9_0.bin, 512, fixed-<reserved>-0, 694898d1c345bdb31b377790ed7fc0b0db184bf7
writing item=1, 9:0:primary_gpt, 512, 19968, gpt_primary_9_0.bin, 16896, fixed-<reserved>-0, 577cc6c87532c9c1214871dc0ca89531d7af1972
writing item=2, 9:0:A_kernel, 20480, 134217728, boot.img, 53639168, fixed-<reserved>-2, a5d4cdb90cd38d2eea1523953a1e99e071334c4e
QSPI storage size: 67108864 bytes.
Writing A_kernel partition with boot.img
Get size of partition through connection.
53639168 bytes from /mnt/external/boot.img to /dev/nvme0n1: 1KB block=52382 remainder=0
dd if=/mnt/external/boot.img of=/dev/nvme0n1 bs=1K skip=0 seek=20 count=52382
[ 17]: l4t_flash_from_kernel: Successfully flash the emmc
52382+0 records in
52382+0 records out
53639168 bytes (54 MB, 51 MiB) copied, 2.60705 s, 20.6 MB/s
Writing A_kernel partition done
writing item=3, 9:0:A_kernel-dtb, 134238208, 786432, kernel_tegra234-j401-p3768-0000+p3767-0000-recomputer.dtb, 244259, fixed-<reserved>-3, 0436031949dbe890c3c845a6d5c4d47eef77ec17
Writing A_kernel-dtb partition with kernel_tegra234-j401-p3768-0000+p3767-0000-recomputer.dtb
Get size of partition through connection.
244259 bytes from /mnt/external/kernel_tegra234-j401-p3768-0000+p3767-0000-recomputer.dtb to /dev/nvme0n1: 1KB block=238 remainder=547
dd if=/mnt/external/kernel_tegra234-j401-p3768-0000+p3767-0000-recomputer.dtb of=/dev/nvme0n1 bs=1K skip=0 seek=131092 count=238
238+0 records in
238+0 records out
243712 bytes (244 kB, 238 KiB) copied, 0.0135479 s, 18.0 MB/s
dd if=/mnt/external/kernel_tegra234-j401-p3768-0000+p3767-0000-recomputer.dtb of=/dev/nvme0n1 bs=1 skip=243712 seek=134481920 count=547
547+0 records in
547+0 records out
547 bytes copied, 0.00123878 s, 442 kB/s
Writing A_kernel-dtb partition done
writing item=4, 9:0:A_reserved_on_user, 135024640, 33161216, , , fixed-<reserved>-4,
[ 19]: l4t_flash_from_kernel: Warning: skip writing A_reserved_on_user partition as no image is specified
writing item=5, 9:0:B_kernel, 168185856, 134217728, boot.img, 53639168, fixed-<reserved>-5, a5d4cdb90cd38d2eea1523953a1e99e071334c4e
Writing B_kernel partition with boot.img
Get size of partition through connection.
53639168 bytes from /mnt/external/boot.img to /dev/nvme0n1: 1KB block=52382 remainder=0
dd if=/mnt/external/boot.img of=/dev/nvme0n1 bs=1K skip=0 seek=164244 count=52382
52382+0 records in
52382+0 records out
53639168 bytes (54 MB, 51 MiB) copied, 0.411486 s, 130 MB/s
Writing B_kernel partition done
writing item=6, 9:0:B_kernel-dtb, 302403584, 786432, kernel_tegra234-j401-p3768-0000+p3767-0000-recomputer.dtb, 244259, fixed-<reserved>-6, 0436031949dbe890c3c845a6d5c4d47eef77ec17
Writing B_kernel-dtb partition with kernel_tegra234-j401-p3768-0000+p3767-0000-recomputer.dtb
Get size of partition through connection.
244259 bytes from /mnt/external/kernel_tegra234-j401-p3768-0000+p3767-0000-recomputer.dtb to /dev/nvme0n1: 1KB block=238 remainder=547
dd if=/mnt/external/kernel_tegra234-j401-p3768-0000+p3767-0000-recomputer.dtb of=/dev/nvme0n1 bs=1K skip=0 seek=295316 count=238
238+0 records in
238+0 records out
243712 bytes (244 kB, 238 KiB) copied, 0.00660128 s, 36.9 MB/s
dd if=/mnt/external/kernel_tegra234-j401-p3768-0000+p3767-0000-recomputer.dtb of=/dev/nvme0n1 bs=1 skip=243712 seek=302647296 count=547
547+0 records in
547+0 records out
547 bytes copied, 0.00103862 s, 527 kB/s
Writing B_kernel-dtb partition done
writing item=7, 9:0:B_reserved_on_user, 303190016, 33161216, , , fixed-<reserved>-7,
[ 19]: l4t_flash_from_kernel: Warning: skip writing B_reserved_on_user partition as no image is specified
writing item=8, 9:0:recovery, 336351232, 83886080, recovery.img, 59107328, fixed-<reserved>-8, 68162e113694e637d0241f07ac56e42ec58f8349
Writing recovery partition with recovery.img
Get size of partition through connection.
59107328 bytes from /mnt/external/recovery.img to /dev/nvme0n1: 1KB block=57722 remainder=0
dd if=/mnt/external/recovery.img of=/dev/nvme0n1 bs=1K skip=0 seek=328468 count=57722
57722+0 records in
57722+0 records out
59107328 bytes (59 MB, 56 MiB) copied, 2.77829 s, 21.3 MB/s
Writing recovery partition done
writing item=9, 9:0:recovery-dtb, 420237312, 524288, tegra234-j401-p3768-0000+p3767-0000-recomputer.dtb.rec, 244259, fixed-<reserved>-9, 0436031949dbe890c3c845a6d5c4d47eef77ec17
Writing recovery-dtb partition with tegra234-j401-p3768-0000+p3767-0000-recomputer.dtb.rec
Get size of partition through connection.
244259 bytes from /mnt/external/tegra234-j401-p3768-0000+p3767-0000-recomputer.dtb.rec to /dev/nvme0n1: 1KB block=238 remainder=547
dd if=/mnt/external/tegra234-j401-p3768-0000+p3767-0000-recomputer.dtb.rec of=/dev/nvme0n1 bs=1K skip=0 seek=410388 count=238
238+0 records in
238+0 records out
243712 bytes (244 kB, 238 KiB) copied, 0.0131009 s, 18.6 MB/s
dd if=/mnt/external/tegra234-j401-p3768-0000+p3767-0000-recomputer.dtb.rec of=/dev/nvme0n1 bs=1 skip=243712 seek=420481024 count=547
547+0 records in
547+0 records out
547 bytes copied, 0.0013336 s, 410 kB/s
Writing recovery-dtb partition done
writing item=10, 9:0:esp, 420761600, 67108864, esp.img, 67108864, fixed-<reserved>-10, b918effc220a23e314a75a5c650564aa001143f8
Writing esp partition with esp.img
Get size of partition through connection.
67108864 bytes from /mnt/external/esp.img to /dev/nvme0n1: 1KB block=65536 remainder=0
dd if=/mnt/external/esp.img of=/dev/nvme0n1 bs=1K skip=0 seek=410900 count=65536
65536+0 records in
65536+0 records out
67108864 bytes (67 MB, 64 MiB) copied, 3.1546 s, 21.3 MB/s
Writing esp partition done
writing item=11, 9:0:recovery_alt, 487870464, 83886080, , , fixed-<reserved>-11,
[ 25]: l4t_flash_from_kernel: Warning: skip writing recovery_alt partition as no image is specified
writing item=12, 9:0:recovery-dtb_alt, 571756544, 524288, , , fixed-<reserved>-12,
[ 25]: l4t_flash_from_kernel: Warning: skip writing recovery-dtb_alt partition as no image is specified
writing item=13, 9:0:esp_alt, 572280832, 67108864, , , fixed-<reserved>-13,
[ 25]: l4t_flash_from_kernel: Warning: skip writing esp_alt partition as no image is specified
writing item=14, 9:0:UDA, 639401984, 419430400, , , fixed-<reserved>-14,
[ 25]: l4t_flash_from_kernel: Skip writing UDA partition
writing item=15, 9:0:reserved, 1058832384, 502792192, , , fixed-<reserved>-15,
[ 25]: l4t_flash_from_kernel: Warning: skip writing reserved partition as no image is specified
writing item=16, 9:0:APP, 1561624576, 100838354944, , , expand-<reserved>-1,
Formatting APP partition /dev/nvme0n1p1 ...
mke2fs 1.46.5 (30-Dec-2021)
Discarding device blocks: done
Creating filesystem with 487997385 4k blocks and 122003456 inodes
Filesystem UUID: 6b281cb1-1fc2-4fce-b268-f675e42c742f
Superblock backups stored on blocks:
32768, 98304, 163840, 229376, 294912, 819200, 884736, 1605632, 2654208,
4096000, 7962624, 11239424, 20480000, 23887872, 71663616, 78675968,
102400000, 214990848
Allocating group tables: done
Writing inode tables: done
Creating journal (262144 blocks): done
Writing superblocks and filesystem accounting information: done
Formatting APP parition done
Formatting APP partition /dev/nvme0n1p1 ...
tar -x -I 'zstd -T0' -pf /mnt/external/system.img --checkpoint=10000 --warning=no-timestamp --numeric-owner --xattrs --xattrs-include=* -C /tmp/ci-3JxyTwa8t7
tar: Read checkpoint 10000
tar: Read checkpoint 20000
tar: Read checkpoint 30000
tar: Read checkpoint 40000
tar: Read checkpoint 50000
tar: Read checkpoint 60000
tar: Read checkpoint 70000
tar: Read checkpoint 80000
tar: Read checkpoint 90000
tar: Read checkpoint 100000
tar: Read checkpoint 110000
Erased 67108864 bytes from address 0x00000000 in flash
Flash index file is /mnt/internal/flash.idx
Number of lines is 61
max_index=60
Flash failure
Either the device cannot mount the NFS server on the host or a flash command has failed. Debug log saved to /tmp/tmp.cm1A0qMb7s. You can access the target's terminal through "sshpass -p root ssh root@fc00:1:1:0::2"
Cleaning up...