Female 7-pin header sockets for Xiao - Supplier and part number?

It looks like I’m going to have to make a custom board to finish my project, but I’m having great difficulty tracking down the correct female headers. The Grove shield has 2 x 7 socket, 4mm high female headers so I presume Seeed must be sourcing them from somewhere. Where that “somewhere” is is proving impossible to find. Does anyone know the manufacturer and part numbers for these?

I can find 8mm high sockets and 1.27mm high sockets but both of these cause other problems with finding pogo pins of the correct lengths and in fitting the board into the case. On the Grove shield, the base of the Xiao board sits 8mm above the shield PCB and I want to replicate that spacing.

P.S, I am lousy at soldering so I plan to have the boards built for me. I would struggle badly to solder in my own headers.

I tend to stick with the standard height 2.54mm Pin Header (Female). I found the shorter connectors to be unreliable, especially those on the XIAO Expansion Board (with Pogo Pins).
If you want good quality use round pins and receptacles, preferably gold plated.

Re sources. It depends where you’re planning to have the board/s assembled.

Re assembly. As you’re having the board/s assembled, and want to use the underside pads on the XIAO, I’d recommend going “surface mount”. Pogo’s are really useful for testing, not sure on long term use.

Thanks for the response, The board I need is incredibly simple. It just consists of a Grove connector, a battery connector, a socket for a Xiao nRF54LM20A and two pogo pings to reach the Xiao’s power pads. I only need it because, as I finally discovered, the Grove shield that I was using and the nRF54 aren’t compatible when it comes to power management: the shield’s power management is flaky, and the nRF54’s built in chip needs power fed directly to the pads. I think surface mounting would be overkill, plus it wouldn’t reuse the existing components that I have. This is a hobby project, so pogo pins will be absolutely fine.

Hi there,

Solder or something very steady will be needed, Any fudgery on the MCU’s power will glitch you to reset a lot so maybe a socket?

You can see several PCB I had made on here in some other threads, For the Battery Soldering IS the most reliable, The Socket works well and is still working on the prototype I made that uses it, biggest issue is “Moving” the Pads’ Seeed :backhand_index_pointing_left: :grin:

HTH
GL :slight_smile: PJ :v:

You can see how the sockets are made, and Add pins where you need. there is a video of it on here. :+1:

Nice! Unfortunately I don’t have a 3D printer. (This is the subject of ongoing domestic negotiations.) In fact, I don’t even have a workbench, just a desk. My plan was to build my project Lego-style as much as possible so as to avoid the need to solder. I think I may have to bite the bullet and use taller sockets with longer pogos. This will mean sacrificing the case that cost me a small fortune because, again, I don’t have a 3D printer.

Thanks for the response. I have a better understanding of your requirements now.

Pogos (eg Harwin) and Connectors (eg Samtec) are available from a number of suppliers - just depends where you are purchasing from.

Pogos can vary in height and contact point type. For power I generally use “castle” - more contact points.

These are the connectors I use.

These are the Pogos I (sometimes) use.

PS> The trick that worked for me re the 3D printer was showing and then printing the wife things she could use, eg phone holder for desk and car, plant trellises, kitchen “helpers”, drawer organisers :wink:

Thanks, that was really useful. (The headers&pins, that is, not the domestic negotiations! :grin:)

I saw those, but I need the female ones.

yes… i noticed the female doesn not show in the search… I have reached out to seeed about this..

There are US, UK and EU suppliers that may be easier than using a PRC source. I’d go with Mouser, Digikey or Element14 for small quantities…

Hi there,

Well, Ok. @grobasoz has you covered on the hardware angle and partial on the other.
I admit it, I salted the deck at my house, I was playing a lot of youtube 3D printing video’s back when the 3D printers really started to come to makers, one at home was “WHAT” ? WHY ? :grin:

Somehow, an Ender 3Pro showed up for my Bday one year, and the FitBit holder (hers)I printed, I already know how far it is, :wink: :v: and then the “SPICE Rack” brackets and HF mag-strip, printed next, HERE"S the VIDEO btw.. for the dates, 5-6 years at least ? sealed the deal. :people_hugging:
:drooling_face:Yea 5 printers later…I see color so.
Keep trying ,eHmm’ a.k.a.(negotiating)

Small Plasma cutter table coming up same way. for metal parts though…:+1:

HTH
GL :slight_smile: PJ :v:

One thing worth checking is the required mating height, not just the 7-pin count and pitch. On the XIAO, the available clearance can make otherwise compatible headers unsuitable. You have to compare the header height against the board, any attached expansion board, and the intended mating connector before ordering. Has anyone found a specific part that fits the XIAO while maintaining the required clearance?

Yes, and discovered the hard way. My pogo pins came up 0.5mm too short. My bodged but working solution is a blob of solder on each of the battery pads on the bottom of the chip.

(There’s a l-o-n-g and continuing story about my attempts to make my first PCB. I will write up at a later date.)

That 0.5 mm difference can make a surprisingly big difference with pogo pins. The solder blobs are a clever workaround, especially for getting the prototype working.

Just started my xiao project. Quick question about the header: on either side, there are 2 two rows of through holes, one with full round holes and the other row with half circle holes at the edge. Why’s that? What’s the purpose of the half circle holes? How to use them? I assume the default way is to use the full round holes, right? Is the spacing between two full holes 0.6 inches? Is there any existing standard proto board coming with two female headers and breadboard style traces? Thanks a lot for your time reading my questions.

If anyone is still interested, I blogged about this problem here:

Hi there,

AND Welcome Here…

So, To answer your questions:

  • What are the half-circle holes? Those are called castellated holes (or castellated mounting pads). They are standard plated through-holes that get cut in half during PCB panel milling, leaving exposed, plated copper edges on the sides and bottom.

  • Why have both? Flexibility.

    • The full round holes are standard 2.54 mm (0.1") pitch through-holes for standard pin headers or socket strips—perfect for breadboarding and prototyping.

    • The castellated edges let the XIAO be used like a surface-mount module (SMD). You can lay the XIAO flat directly onto a custom PCB carrier without any through-hole pins sticking through the bottom, soldering the edges directly down like a stamp. This keeps vertical clearance practically flush.

  • The unexpected advantage: Beyond surface mounting, those castellated notches give you positive mechanical alignment. In fact, I designed a 3D-printed socket here on the forum that takes advantage of the XIAO’s exterior dimensions and those castellations to pressure-fit / snap the board firmly into place without needing permanent solder or extra fasteners. It makes swapping modules quick and holds everything secure.

  • Pin spacing & boards: Yes, the spacing between the two 7-pin rows is 0.6 inches (15.24 mm), making it a standard DIP-14 width. It fits standard breadboards (spanning the center groove) and any standard 0.6" wide proto-board layout. Seeed also makes the Seeed Studio Expansion Board for XIAO (and several third-party breakout boards) that already include pre-soldered female sockets, Grove connectors, and power circuitry out of the box.

HTH
GL :slight_smile: PJ :v:


I used the geometry to bite into the pins. :+1:
:wink:
https://forum.seeedstudio.com/t/another-xiao-socket-adapter-revision-iii/266872?u=pj_glasso

Look at the 7-pin female header sockets that come with the RGB matrix. Seeed must have them, seems odd they don’t sell them separately. https://www.seeedstudio.com/6x10-RGB-MATRIX-for-XIAO-p-5771.html

I agree that it’s odd but I - or, rather, Claude- did eventually find some.