Summary
In seeedstudio page, there is the following description.
- Ubuntu Host PC (native or VM using VMware Workstation Player)
So, I installed “Jetson Linux” to reComputer J4012 using VMware Workstation Player.
But, I could NOT shutdown reComputer J4012 after this installation.
On the other hands, I could shutdown reComputer J4012 when I used native Ubuntu Host PC(not VM) to flash Jetson Linux.
Environment
- reComputer J4012(Jetson Orin NX 16GB)
- Jetson Linux 35.3.1 https://developer.nvidia.com/embedded/jetson-linux-r3531
Steps to reproduce
Host PC(x86_64)
tar xf Jetson_Linux_R35.3.1_aarch64.tbz2
sudo tar xpf Tegra_Linux_Sample-Root-Filesystem_R35.3.1_aarch64.tbz2 -C Linux_for_Tegra/rootfs/
cd Linux_for_Tegra/
sudo ./apply_binaries.sh
sudo ./tools/l4t_flash_prerequisites.sh
sudo ./tools/kernel_flash/l4t_initrd_flash.sh --external-device nvme0n1p1 \
-c tools/kernel_flash/flash_l4t_external.xml -p "-c bootloader/t186ref/cfg/flash_t234_qspi.xml" \
--showlogs --network usb0 p3509-a02+p3767-0000 internal
reComputer J4012
sudo shutdown -h now