🤩 Exciting new features in nRF Connect SDK 3.2.0

Opposite of the Others Nordic is Bringing it…

:grin: :oncoming_fist:
In this webinar, The Dev talks about the exciting new features of the latest nRF Connect SDK release, including nRF Connect SDK bare metal option, with demo showcasing.

nRF Connect SDK is Nordic’s software development kit for Bluetooth® Low Energy, Bluetooth® Mesh, Zigbee, Thread, Matter, Wi-Fi, and cellular IoT applications. nRF Connect SDK is a comprehensive and scalable solution that supports our nRF52, nRF53, nRF54, nRF70 and nRF91 Series devices.

00:00 - Intro and agenda
01:28 - Generic Updates
09:33 - Bluetooth Updates
17:15 - Demo: Bluetooth Shorter Connection Intervals (SCI)
21:58 - Wi-Fi Updates
23:31 - Matter Updates
28:54 - Demo: Matter Quick Start application
34:33 - Cellular IoT Updates
37:58 - nRF Connect SDK Bare Metal option updates
41:53 - Demo: S145 SoftDevice (multirole central and peripheral)
46:01 - Closing and Q&A

DFU, single slot OTA over BLE , Bare Metal :heart_eyes:

Check it out NOW!

HTH
GL :slight_smile: PJ :v:

Hi,

Thanks for sharing this.

Does it compile correctly without errors with this version 3.2.0 of the SDK for the XIAO nRF54L15 board?

Regards

Hi there,

Yes, no Issues’ with the Basics, However it’s moot as they have just updated to 3.2.1 so include some refreshes to be more in line with the Zephyr upstream * nRF54L Series:

  • Added experimental support for nRF54LM20A Engineering B.

Probably have a improved the Soft devices also.

Fuzola, Back to retest again… Standby :+1:

HTH
GL :slight_smile: PJ :v:

EDIT: ADD,
the Build would crash under the new toolchain and SDK, until I stopped forcing the Board root to the Seeed one, Not using the Switch It compiles AOK, the “WatchFace Demo” works with Round display.
From this:

PS D:\Nordic\myapps\workspace\watchface> west build -p always -d build_periph -b xiao_nrf54l15/nrf54l15/cpuapp -- `
>>   -DBOARD_ROOT="C:/ncs/Seeed/platform-seeedboards/zephyr" `
>>   -DSHIELD=seeed_xiao_expansion_board
-- west build: making build dir D:\Nordic\myapps\workspace\watchface\build_periph pristine
-- west build: generating a build system

To this: :+1:

west build -p always -d build_periph -b xiao_nrf54l15/nrf54l15/cpuapp -- -DSHIELD=seeed_xiao_expansion_board

[614/614] Linking C executable zephyr\zephyr.elf
Memory region Used Size Region Size %age Used
FLASH: 520236 B 1428 KB 35.58%
RAM: 30888 B 188 KB 16.04%
IDT_LIST: 0 GB 32 KB 0.00%
Generating files from D:/Nordic/myapps/workspace/watchface/build_periph/watchface/zephyr/zephyr.elf for board: xiao_nrf54l15
[10/10] Generating ../merged.hex
PS D:\Nordic\myapps\workspace\watchface>

I may also add I did update VS code to the latest Dec release also. just FYI.
so I think also the Zephyr is upstream is up to date with the latest :crossed_fingers: date also.

And none of these updates, at least the essential ones (like bluetooth schorter intervals, single slot OTA), are not for the older chips, like nrf52840, unfortunately :frowning:

Hi there,

Yes, Sir You are Correct :grin: However, The next Softdevice version for the nRF52840 will have some updates too very, soon. :+1:

While speaking to the Vikings, I got that they want BareMetal to be Stable with it’s own Softdevice initially, then they have a plan to converge to a new softDevice covering all the Nrf52 & 54 series unfortunately the Nrf53 series is the “red Headed Step child” or something it’s really the only True Dual Core too!, all this LP core bahlony IMO, hard to code and info is limited!.

STay tuned, and WOW the M variant is going to be BANANAS :grin:

HTH
GL :slight_smile: PJ :v:

BTW , single slot OTA was never a thing for Xiao nRF52840 , because the external flash was there and big, MCU boot with crashproof DFU is available for the 52 series FWIW :v:
the SI is a New BLE spec piece so wouldn’t have applied anyway without a Newer Softdevice.

It’s not all bad News :grin: +

, SO if you build with the newer toolchain and SDK you will use less RAM and Flash
which is always a step in the right direction. :+1:

Yep, I moved to the 3.2 SDK and Toolchain for my nrf52840 project. Anyway, I think if I would like to migrate to nrf54 it will be an easy migration.