I’m looking for a way to do a software reboot on an ESP32C6. The context is that this is a reboot after a factory reset and wipe of configuration data. My research says that this is achieved by calling NVIC_SystemReset() but the Arduino IDE says this isn’t defined. (“Compilation error: ‘NVIC_SystemReset’ was not declared in this scope”). I can’t find which header file this function is declared in. Is it somewhere that’s not obvious, or is there a deeper problem in that the function isn’t defined for the ESP32C6? The Seeed wiki doesn seem to have anything relevant. Any pointers/help would be greatly appreciated.
Please try
ESP.restart().
EDIT
[Note]:I tried it, but after executing ESP.restart(); two or three times, C6 hangs up. To start it up, I need to re-upload the sketch. The cause is still unknown.
Simple code seems to restart without any problems.
void setup() {
Serial.begin(115200);
delay(1000);
pinMode(LED_BUILTIN, OUTPUT);
}
void loop() {
for(int i = 0; i < 10; i++) {
digitalWrite(LED_BUILTIN, LOW);
delay(200);
digitalWrite(LED_BUILTIN, HIGH);
delay(200);
}
Serial.println("Restarting now...");
delay(1000);
ESP.restart();
}
Many thanks. I’ve not found this call documented anywhere else so this is a good find for me. I tried it, and it works. It’s for a feature that I don’t expect to be used very often and it’s not for a commercial product, so having to re-upload occasionally isn’t a problem.
Hi there,
What about going to Deep sleep with no-time/very sort timer wake-up? . (where it goes to sleep and wakes right up) Would it not start from reset? like the Nrf52840 Xiao, maybe.
HTH
GL
PJ ![]()
I tried it, and it restarts without any problems either way.
esp_sleep_enable_timer_wakeup(1);
esp_deep_sleep_start();
ESP.restart();