Hi,
I have been creating a small HomeKit sensor that combines the Xiao-esp32c3 and a MR24HPC1 sensor using Homespan. I have been trundling along quite well with development, but now have an issue that after I upload my code, the esp32c3 goes into an endless reboot, with the following being displayed in the terminal after homespan starts up.
ESP-ROM:esp32c3-api1-20210207
Build:Feb 7 2021
rst:0x3 (RTC_SW_SYS_RST),boot:0xb (SPI_FAST_FLASH_BOOT)
Saved PC:0x403819b6
SPIWP:0xee
mode:DIO, clock div:1
load:0x3fcd5810,len:0x38c
load:0x403cc710,len:0x6ac
load:0x403ce710,len:0x24e4
entry 0x403cc710
Starting up...
I am developing the solution using Platform.io inside of Visual Studio and read elsewhere that there may be an issue with the uploading configuration, so I added:
board_build.flash_mode = dio
to my platform.ini file, this didn’t solve the problem.
I also read elsewhere that the issue may be due to the strapping pins and that connecting D0 via a 3k3 resistor to USB v5 could resolve the issue. This didn’t work.
Here is the circuit and as can be seen I am not going near the other strapping pins
Has anyone got any clues or ideas as to what to try next?