Hi there!
I am attempting to build a sketch using a static library .a.
I followed this post: Arduino Tutorials - How to Use Static (Pre-compiled) Libraries in Arduino - Seeed Wiki but I got an error during compilation:
Library PrebuiltLib has been declared precompiled:
Using precompiled library in /home/oscar/Arduino/libraries/PrebuiltLib/src/esp32
/tmp/arduino-sketch-9595712C3FF3F4D274F59DD186AB57D9/sketch/src/sensors/SensorA.cpp.o:(.literal._ZN11SensorA3runEb+0x18): undefined reference to `suma'
/tmp/arduino-sketch-9595712C3FF3F4D274F59DD186AB57D9/sketch/src/sensors/SensorA.cpp.o: In function `SensorA::run(bool)':
/home/oscar/App/src/sensors/Sensor.hpp:31: undefined reference to `suma'
collect2: error: ld returned 1 exit status
Error during build: exit status 1
My static library is called PrebuiltLib and has been built for the esp32:esp32:t-beam board. Its source code is:
- PrebuiltLib.h
#ifndef PrebuiltLib_H
#define PrebuiltLib_H
#ifdef __cplusplus
extern "C" {
#endif
int suma (int a, int b);
#ifdef __cplusplus
}
#endif
#endif // PrebuiltLib_H
- PrebuiltLib.c
#include "PrebuiltLib.h"
int suma (int a, int b) {
return a + b;
}
My arduino-cli version is 0.18.3 commit: d710b642.
Before removing the PrebuiltLib.c file, sketch is compiled successfully. When it is removed the error appears.
Oscar