I have Seeed Studio reComputer J2012(Jetson Xavier NX 16GB eMMC), and I want to boot the root from NVMe. at first, the boot was fine then suddenly the artifacts shows on display and the board was crashed. After that, the board is failed to reboot and I want to reflash the board using Jetpack 4.6.1 but always failed with these logs and serial console output: Error - Google Drive
any help to recover my device?