hi i got A608 cariar with jetson orin nx 16
i try to flash and got this problem
[ 4.3885 ] MB2 Applet version 01.00.0000
Board ID(3767) version(300) sku(0000) revision(R.1)
Chip SKU(00:00:00:D3) ramcode(00:00:00:00) fuselevel(fuselevel_production) board_FAB(300)
emc_opt_disable_fuse:(0)
Error: missing cfgfile ().
Usage: sudo ./flash.sh [options] generic internal
options:
-c <cfgfile> ---------- Flash partition table config file.
-d <dtbfile> ---------- device tree file.
-f <flashapp> --------- Path to flash application (tegraflash.py)
-h -------------------- print this message.
-i <enc rfs key file>-- key for disk encryption support.
-k <partition id> ----- partition name or number specified in flash.cfg.
-m <mts preboot> ------ MTS preboot such as mts_preboot_si.
-n <nfs args> --------- Static nfs network assignments
<Client IP>:<Server IP>:<Gateway IP>:<Netmask>
-o <odmdata> ---------- ODM data.
-r -------------------- skip building and reuse existing system.img.
-t <tegraboot> -------- tegraboot binary such as nvtboot.bin
-u <PKC key file>------ PKC key used for odm fused board.
-v <SBK key file>------ Secure Boot Key (SBK) key used for ODM fused board.
-w <wb0boot> ---------- warm boot binary such as nvtbootwb0.bin
-x <tegraid> ---------- Tegra CHIPID.
-B <boardid> ---------- BoardId.
-C <cmdline> ---------- Kernel commandline arguments.
WARNING:
Each option in this kernel commandline gets
higher preference over the values set by
flash.sh. In case of NFS booting, this script
adds NFS booting related arguments, if -i option
is omitted.
-F <flasher> ---------- Flash server such as cboot.bin.
-G <file name> -------- Read partition and save image to file.
-I <initrd> ----------- initrd file. Null initrd is default.
-K <kernel> ----------- Kernel image file such as zImage or Image.
-L <bootloader> ------- Bootloader such as cboot.bin or u-boot-dtb.bin.
-M <mts boot> --------- MTS boot file such as mts_si.
-N <nfsroot> ---------- i.e. <my IP addr>:/my/exported/nfs/rootfs.
-R <rootfs dir> ------- Sample rootfs directory.
-S <size> ------------- Rootfs size in bytes. Valid only for internal
rootdev. KiB, MiB, GiB short hands are allowed,
for example, 1GiB means 1024 * 1024 * 1024 bytes.
-T <ext num sectors> ---The number of the sectors of the external storage device.
The default value is 119537664 if this option is not set.
-U <int num sectors> ---The number of the sectors of the internal storage device.
The default value is 119537664 if this option is not set.
-Z -------------------- Print configurations and then exit.
--no-flash ------------ perform all steps except physically flashing the board.
This will create a system.img.
--external-device------ Generate flash images for external devices
--sparseupdate--------- only flash partitions that have changed. Currently only support SPI flash memory
--no-systemimg -------- Do not create or re-create system.img.
--bup ----------------- Generate bootloader update payload(BUP).
--single-image-bup <part name> Generate specified single image BUP, this must work with --bup.
--bup-type <type> ----- Generate specific type bootloader update payload(BUP), such as bl or kernel.
--multi-spec----------- Enable support for building multi-spec BUP.
--clean-up------------- Clean up BUP buffer when multi-spec is enabled.
--usb-instance <id> --- Specify the USB instance to connect to;
<id> = USB port path (e.g. 3-14).
--no-root-check ------- Typical usage of this script require root permissions.
Pass this option to allow running the script as a
regular user, in which case only specific combinations
of command-line options will be functional.
--uefi-keys <keys_conf> Specify UEFI keys configuration file.
--rcm-boot ------------ Do RCM boot instead of physically flashing the board.
--sign ---------------- Sign images and store them under "bootloader/signed"
directory. The board will not be physically flashed.
--image --------------- Specify the image to be written into board.
--boot-chain-flash <c> Flash only a specific boot chain (ex. "A, "B", "all").
Defaults to "all", inputs are case insensitive.
Not suitable for production.
--boot-chain-select <c> Specify booting chain (ex. "A" or "B") after the board is flashed.
Defaults to "A", inputs are case insensitive.
--pv-crt -------------- The certificate for the key that is used to sign cpu_bootloader
--with-systemimg ------ Generate system images also when using -k option
--pv-enc <enc_key>----- The encryption key that is used to encrypt cpu_bootloader.
--uefi-enc <uefi_enc_key> Key file (0x19: 16-byte; 0x23: 32-byte) to encrypt UEFI payloads
--uda-dir-------------- Directory to store user data that will be encrypted in UDA partition.
--generic-passphrase -- Use generic passphrase for disk encryption.
--disable-random-iv --- Disable generation of random IV, SALT1, SALT2 and DERSTR.
--read-info ----------- Read and display board related info, fuse info (based on fuse_t234.xml),
and EEPROM content.
--reuse-uuid --------- Reuse uuid which is already generated first time.
Error: failed to generate images
Cleaning up...
some time also have problem with boot up but lets start with the first problem … tanks