Dear all.
For this sensor:
I added the library (zip file) from here:
Then I extracted and put it on the libraries.
Then, just when I try to compile the example, I immediately get this msg below.
Do you have an idea about what I am doing wrong?
Could it be something with the library?
Thanks a lot.
Omar Cruz
++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++
Arduino: 1.8.10 (Linux), Board: “Arduino Leonardo”
In file included from /home/o/Downloads/arduino-1.8.10/hardware/arduino/avr/cores/arduino/Arduino.h:30:0,
from /home/o/Arduino/libraries/Grove_-Air_quality_sensor/AirQuality.h:23,
from /home/o/Arduino/libraries/Grove-Air_quality_sensor/examples/AirQuality_Sensor/AirQuality_Sensor.ino:6:
/home/o/Arduino/libraries/Grove-Air_quality_sensor/examples/AirQuality_Sensor/AirQuality_Sensor.ino: In function ‘void TIMER2_OVF_vect()’:
/home/o/Arduino/libraries/Grove-_Air_quality_sensor/examples/AirQuality_Sensor/AirQuality_Sensor.ino:30:5: warning: ‘TIMER2_OVF_vect’ appears to be a misspelled ‘signal’ handler, missing '_vector’ prefix [-Wmisspelled-isr]
ISR(TIMER2_OVF_vect)
^
/home/o/Arduino/libraries/Grove-Air_quality_sensor/AirQuality.cpp: In member function ‘void AirQuality::init(int)’:
/home/o/Arduino/libraries/Grove-Air_quality_sensor/AirQuality.cpp:80:5: error: ‘TCCR2A’ was not declared in this scope
TCCR2A=0;//normal model
^~~~~~
/home/o/Arduino/libraries/Grove-Air_quality_sensor/AirQuality.cpp:80:5: note: suggested alternative: ‘TCCR0A’
TCCR2A=0;//normal model
^~~~~~
TCCR0A
/home/o/Arduino/libraries/Grove-Air_quality_sensor/AirQuality.cpp:81:5: error: ‘TCCR2B’ was not declared in this scope
TCCR2B=0x07;//set clock as 1024*(1/16M)
^~~~~~
/home/o/Arduino/libraries/Grove-Air_quality_sensor/AirQuality.cpp:81:5: note: suggested alternative: ‘TCCR0B’
TCCR2B=0x07;//set clock as 1024*(1/16M)
^~~~~~
TCCR0B
/home/o/Arduino/libraries/Grove-Air_quality_sensor/AirQuality.cpp:82:5: error: ‘TIMSK2’ was not declared in this scope
TIMSK2=0x01;//enable overflow interrupt
^~~~~~
/home/o/Arduino/libraries/Grove-Air_quality_sensor/AirQuality.cpp:82:5: note: suggested alternative: ‘TIMSK0’
TIMSK2=0x01;//enable overflow interrupt
^~~~~~
TIMSK0
Multiple libraries were found for “AirQuality.h”
Used: /home/o/Arduino/libraries/Grove-_Air_quality_sensor
exit status 1
Error compiling for board Arduino Leonardo.
This report would have more information with
“Show verbose output during compilation”
option enabled in File -> Preferences.