Below is the error message I received:
Arduino: 1.6.12 (Windows 10), Board: “Arduino/Genuino Uno”
C:\Program Files (x86)\Arduino\arduino-builder -dump-prefs -logger=machine -hardware C:\Program Files (x86)\Arduino\hardware -hardware C:\Users\Mark Chui\AppData\Local\Arduino15\packages -tools C:\Program Files (x86)\Arduino\tools-builder -tools C:\Program Files (x86)\Arduino\hardware\tools\avr -tools C:\Users\Mark Chui\AppData\Local\Arduino15\packages -built-in-libraries C:\Program Files (x86)\Arduino\libraries -libraries C:\Users\Mark Chui\Documents\Arduino\libraries -fqbn=arduino:avr:uno -vid-pid=0X2A03_0X0043 -ide-version=10612 -build-path C:\Users\MARKCH~1\AppData\Local\Temp\arduino_build_984292 -warnings=none -prefs=build.warn_data_percentage=75 -prefs=runtime.tools.avrdude.path=C:\Users\Mark Chui\AppData\Local\Arduino15\packages\arduino\tools\avrdude\6.3.0-arduino9 -prefs=runtime.tools.arduinoOTA.path=C:\Users\Mark Chui\AppData\Local\Arduino15\packages\arduino\tools\arduinoOTA\1.1.1 -prefs=runtime.tools.avr-gcc.path=C:\Users\Mark Chui\AppData\Local\Arduino15\packages\arduino\tools\avr-gcc\4.9.2-atmel3.5.4-arduino2 -verbose C:\Users\Mark Chui\Documents\Arduino\Gardening_demo_Arduino\Gardening\Gardening.ino
C:\Program Files (x86)\Arduino\arduino-builder -compile -logger=machine -hardware C:\Program Files (x86)\Arduino\hardware -hardware C:\Users\Mark Chui\AppData\Local\Arduino15\packages -tools C:\Program Files (x86)\Arduino\tools-builder -tools C:\Program Files (x86)\Arduino\hardware\tools\avr -tools C:\Users\Mark Chui\AppData\Local\Arduino15\packages -built-in-libraries C:\Program Files (x86)\Arduino\libraries -libraries C:\Users\Mark Chui\Documents\Arduino\libraries -fqbn=arduino:avr:uno -vid-pid=0X2A03_0X0043 -ide-version=10612 -build-path C:\Users\MARKCH~1\AppData\Local\Temp\arduino_build_984292 -warnings=none -prefs=build.warn_data_percentage=75 -prefs=runtime.tools.avrdude.path=C:\Users\Mark Chui\AppData\Local\Arduino15\packages\arduino\tools\avrdude\6.3.0-arduino9 -prefs=runtime.tools.arduinoOTA.path=C:\Users\Mark Chui\AppData\Local\Arduino15\packages\arduino\tools\arduinoOTA\1.1.1 -prefs=runtime.tools.avr-gcc.path=C:\Users\Mark Chui\AppData\Local\Arduino15\packages\arduino\tools\avr-gcc\4.9.2-atmel3.5.4-arduino2 -verbose C:\Users\Mark Chui\Documents\Arduino\Gardening_demo_Arduino\Gardening\Gardening.ino
Using board ‘uno’ from platform in folder: C:\Users\Mark Chui\AppData\Local\Arduino15\packages\arduino\hardware\avr\1.6.21
Using core ‘arduino’ from platform in folder: C:\Users\Mark Chui\AppData\Local\Arduino15\packages\arduino\hardware\avr\1.6.21
Detecting libraries used…
“C:\Users\Mark Chui\AppData\Local\Arduino15\packages\arduino\tools\avr-gcc\4.9.2-atmel3.5.4-arduino2/bin/avr-g++” -c -g -Os -w -std=gnu++11 -fpermissive -fno-exceptions -ffunction-sections -fdata-sections -fno-threadsafe-statics -flto -w -x c++ -E -CC -mmcu=atmega328p -DF_CPU=16000000L -DARDUINO=10612 -DARDUINO_AVR_UNO -DARDUINO_ARCH_AVR “-IC:\Users\Mark Chui\AppData\Local\Arduino15\packages\arduino\hardware\avr\1.6.21\cores\arduino” “-IC:\Users\Mark Chui\AppData\Local\Arduino15\packages\arduino\hardware\avr\1.6.21\variants\standard” “C:\Users\MARKCH~1\AppData\Local\Temp\arduino_build_984292\sketch\Gardening.ino.cpp” -o “nul”
“C:\Users\Mark Chui\AppData\Local\Arduino15\packages\arduino\tools\avr-gcc\4.9.2-atmel3.5.4-arduino2/bin/avr-g++” -c -g -Os -w -std=gnu++11 -fpermissive -fno-exceptions -ffunction-sections -fdata-sections -fno-threadsafe-statics -flto -w -x c++ -E -CC -mmcu=atmega328p -DF_CPU=16000000L -DARDUINO=10612 -DARDUINO_AVR_UNO -DARDUINO_ARCH_AVR “-IC:\Users\Mark Chui\AppData\Local\Arduino15\packages\arduino\hardware\avr\1.6.21\cores\arduino” “-IC:\Users\Mark Chui\AppData\Local\Arduino15\packages\arduino\hardware\avr\1.6.21\variants\standard” “-IC:\Users\Mark Chui\AppData\Local\Arduino15\packages\arduino\hardware\avr\1.6.21\libraries\Wire\src” “C:\Users\MARKCH~1\AppData\Local\Temp\arduino_build_984292\sketch\Gardening.ino.cpp” -o “nul”
“C:\Users\Mark Chui\AppData\Local\Arduino15\packages\arduino\tools\avr-gcc\4.9.2-atmel3.5.4-arduino2/bin/avr-g++” -c -g -Os -w -std=gnu++11 -fpermissive -fno-exceptions -ffunction-sections -fdata-sections -fno-threadsafe-statics -flto -w -x c++ -E -CC -mmcu=atmega328p -DF_CPU=16000000L -DARDUINO=10612 -DARDUINO_AVR_UNO -DARDUINO_ARCH_AVR “-IC:\Users\Mark Chui\AppData\Local\Arduino15\packages\arduino\hardware\avr\1.6.21\cores\arduino” “-IC:\Users\Mark Chui\AppData\Local\Arduino15\packages\arduino\hardware\avr\1.6.21\variants\standard” “-IC:\Users\Mark Chui\AppData\Local\Arduino15\packages\arduino\hardware\avr\1.6.21\libraries\Wire\src” “C:\Users\MARKCH~1\AppData\Local\Temp\arduino_build_984292\sketch\Gardening.ino.cpp” -o “C:\Users\MARKCH~1\AppData\Local\Temp\arduino_build_984292\preproc\ctags_target_for_gcc_minus_e.cpp”
C:\Users\Mark Chui\Documents\Arduino\Gardening_demo_Arduino\Gardening\Gardening.ino:31:23: fatal error: SeeedOLED.h: No such file or directory
#include <SeeedOLED.h>
^
compilation terminated.
Using library Wire at version 1.0 in folder: C:\Users\Mark Chui\AppData\Local\Arduino15\packages\arduino\hardware\avr\1.6.21\libraries\Wire
exit status 1
Error compiling for board Arduino/Genuino Uno.
============================================
I tried looking under the directory that they suggested but was unable to find it
Am I suppposed to manually add the SeeedOLED folder or change the code in the sketch itself?
Hi , please download <LINK_TEXT text=“https://github.com/Seeed-Studio/OLED_Di … master.zip”>https://github.com/Seeed-Studio/OLED_Display_128X64/archive/master.zip</LINK_TEXT> library and then follow <LINK_TEXT text=“http://wiki.seeedstudio.com/How_to_inst … o_Library/”>http://wiki.seeedstudio.com/How_to_install_Arduino_Library/</LINK_TEXT> to add the oled library. thanks.
Seeed techsupport team
Bill