error collecting microphone data in EDGE IMPULSE

Hi: When connect the XIAO 52840 sense microphone with “edge-impulse-data-forwarder” and try to use data acquisition i get the error: Invalid data collected from device. Also on Collect data section i see Sensor: Sensor with 1 axes Frequency: 2646Hz. On the logs appear: Failed to sample data Error: Invalid data collected from device. All values should be numeric, and every line should have 1 value. Can you please help me?