EN05 HelloWorld sample compilation failure

I’m using an EN05 ePaper board (with the nRF52840)

I’ve installed the GFX library (today!) and the HelloWorld example compiles when opened.

Once I add the driver.h file and fill it with this:

#define BOARD_SCREEN_COMBO 508 // 2.13 inch monochrome ePaper Screen (SSD1680)
#define USE_XIAO_EPAPER_DISPLAY_BOARD_EN05

compilation fails with stuff like this

In file included from h:\Sketches\libraries\Seeed_GFX/User_Setups/Setup508_Seeed_XIAO_EPaper_2inch13.h:21,
                 from h:\Sketches\libraries\Seeed_GFX/User_Setups/Dynamic_Setup.h:301,
                 from h:\Sketches\libraries\Seeed_GFX/User_Setup_Select.h:13,
                 from h:\Sketches\libraries\Seeed_GFX\TFT_eSPI.h:69,
                 from h:\Sketches\libraries\Seeed_GFX\TFT_eSPI.cpp:16:
h:\Sketches\libraries\Seeed_GFX\TFT_eSPI.cpp: In member function 'void TFT_eSPI::initBus()':
h:\Sketches\libraries\Seeed_GFX/User_Setups/EPaper_Board_Pins_Setups.h:69:16: error: 'D16' was not declared in this scope; did you mean 'D10'?
   69 | #define TFT_DC D16  // D16
      |                ^~~
h:\Sketches\libraries\Seeed_GFX\TFT_eSPI.cpp:576:7: note: in expansion of macro 'TFT_DC'
  576 |   if (TFT_DC >= 0) {
      |       ^~~~~~
h:\Sketches\libraries\Seeed_GFX/User_Setups/EPaper_Board_Pins_Setups.h:71:17: error: 'D11' was not declared in this scope; did you mean 'D10'?
   71 | #define TFT_RST D11 // D11
      |                 ^~~
h:\Sketches\libraries\Seeed_GFX\TFT_eSPI.cpp:583:7: note: in expansion of macro 'TFT_RST'
  583 |   if (TFT_RST >= 0) {
      |       ^~~~~~~
In file included from h:\Sketches\libraries\Seeed_GFX\TFT_eSPI.h:30,
                 from h:\Sketches\libraries\Seeed_GFX\TFT_eSPI.cpp:16:
h:\Sketches\libraries\Seeed_GFX\TFT_eSPI.cpp: In member function 'void TFT_eSPI::initFromSleep(uint8_t)':
h:\Sketches\libraries\Seeed_GFX/User_Setups/EPaper_Board_Pins_Setups.h:69:16: error: 'D16' was not declared in this scope; did you mean 'D10'?

I’ve selected the nRF52840 Sense as per the instructions

Any ideas?

Hi there,

So it looks like it is complaining about TFT-eSPI.sys not having the right user select settings correct to match the board , open that file and be sure only one is selected,

HTH
GL :slight_smile: PJ :v: