Elp Needed: Setting Up Analog Microphone and Speaker on Jetson Orin NX (A608 Carrier)

Hello everyone,

I’m running into some issues with audio configuration on my Jetson Orin NX (16GB) with Ubuntu 20.04 and JetPack 5.1.2. I’m using the A608 carrier board from Seeed Studio, and I’m trying to connect an analog microphone (connected to W33) and a speaker (connected to W10), both of which are amplified. I’ve tested the microphone on a standard computer with a 3.5mm jack, and it works fine, so the hardware itself is functional.

Issues I’m Facing:

  1. Device Not Recognized: The Jetson doesn’t seem to recognize either the microphone or the speaker when connected to the specified ports (W33 and W10).
  2. AUX Port Pop-Up Issue: When I connect any hardware to the 3.5mm AUX port, an audio application in Ubuntu repeatedly pops up, which is a minor inconvenience but worth mentioning.

My main goal is to get the analog microphone and speaker working correctly on the Jetson via W33 and W10. I’d appreciate any guidance on configuring this setup—specific driver suggestions, configuration steps, or any similar experiences with solutions.

Thanks in advance for your help!