I am looking to use the Ethernet capabilities of the EdgeBox-ESP-100. Do you have any Ethernet examples you can share? Specifically, I would like to get the MAC address programmatically then pass the MAC to the Ethernet.begin(mac) function. Also, are there any special Ethernet libraries that need to be used with this device instead of the Arduino Ethernet? Thanks for your help.
Regards, Mark