I’m not sure how to use the 8MB PSRAM on EdgeBox-ESP-100:
The schematic says…
From ESP32S3 Series Datasheet:
Octal SPI occupies five more GPIOs (GPIO33 ∼ GPIO37) than Quad SPI
The 8MB internal PSRAM is using Octal SPI according to the datasheet.
I’m not sure how to use the 8MB PSRAM on EdgeBox-ESP-100:
The schematic says…
From ESP32S3 Series Datasheet:
Octal SPI occupies five more GPIOs (GPIO33 ∼ GPIO37) than Quad SPI
The 8MB internal PSRAM is using Octal SPI according to the datasheet.
For example, I’m flashing the regular version of MicroPython v1.22.2 (2024-02-22) for ESP32-S3.
This firmware supports configurations with and without SPIRAM (also known as PSRAM) and will auto-detect a connected SPIRAM chip at startup and allocate the MicroPython heap accordingly. However if your board has Octal SPIRAM, then use the “spiram-oct” variant.
When using regular variant:
>>> gc.mem_free()
250816
When using “spiram-oct” variant:
>>> gc.mem_free()
8320144
But obviously, I can’t use DO3, DO4, DO5 when using PSRAM
Sorry I’m late. When using PSRAM, those 3 I/O pins become unavailable. Only when not using PSRAM can those three I/O pins be used.
We will try to find and send you the usage method for PSRAM. Thank you for your patience and support.