When I connect the controller in the socket of the test arms then sometimes goes the startup wrong.
We see the:
- the MiniWare log
- DT71 V1.08
- and then switch it continue between the submenu (started with Identify), touching the button does not stop this scrolling.
Only disconnection en reconnection can help.
I have cleaned the touch button, without any sucess.
In a normal startup is the working as descripted in the user manual.