Try them in the order i posted them starting with 4 then 411 and finally 420 only install one at a time then try it and if it dont work on to the next im going to add one last file try this one first acually its the ben f for the 3.22 boot loader it will be the best for functionality if it will take if not then try the factory ones. The files with 2 files need to both be installed one after another and make sure the file changes to the dry extension. Dont stress its will be solved ![]()
BenF364_LIB353-1.zip (49.6 KB)
201V4_20.zip (39.3 KB)
201V4-11.zip (31.5 KB)
DS201V4.zip (41.2 KB)