my computer will not recognize dso nano on usb i hold down button turn on and
it does nothinf john scully
Not enough information provided. Tell us what you are trying to do, which operating system you have, and what applications have been installed to support what you are trying to do.
My car isn’t running, please tell me what is wrong with my car. See what I mean? ![]()
i have windows vista basic im just trying to operate the usb bus
what do i need john s.
My USB bus isn’t running, please tell me what is wrong with my USB bus.
What are you trying to do with the Nano USB port?
Probably the same thing as your car … have you considered a correlation between the two here ![]()
Pete
WHAT DO I NEED TO RUN MY DSO NANO WTH USB BUS NEED SUPPORT
CALL 508-886-2988
Hello,
First of all, please don’t capitalize, it’s considered yelling on all forums and chats.
You can start by looking around the forum, but a quick DSO nano introduction is like this:
use dfuse for firmware upgrades (should work on all windows OS)
this is the latest independent firmware that most of the people on this forum agree it’s really good to use
here you can find some old documents/firmware if you don’t like the latest one
As a final note, this is a scope mostly for amateurs/hackers so a bit of self investigating and individual trial and error is expected from everyone.
The Nano USB port acts as two separate entities. It can be a normal SD card reader while in normal mode, or it can be an upgrade port when used to update firmware. You have still failed to specified which you are trying to do.