Does there any module you have it that support read/ write RFID tag at one source code

Does there any module you have it that support read/ write RFID tag at one source code, in this moment I use two RFID modules one for read and other one for Write. If you have please mention the module or give me a link that available in Russia.

Hi there,


1. Please check if Grove-NFC meets your requirement. http://wiki.seeedstudio.com/Grove_NFC/

2. For the Russian distributor, you can refer to https://www.seeedstudio.com/distributors.html

Thanks

best rgds
Bill

It does not work with Arduino Mega 2560 R3, I did solid four pins for GNU VCC TX RX and connected with 20, 21 nothing? any idea!!

Hi there,We suggest UART(by default) to communicate with Mega. So you have to use the TX of NFC to RX of Mega(such as 19/17/15), and RX of NFC to TX of Meag(such as 18/16/14). thanks.



BOARD

USB CDC NAME

SERIAL PINS

SERIAL1 PINS

SERIAL2 PINS

SERIAL3 PINS





Uno, Nano, Mini



0(RX), 1(TX)





Mega



0(RX), 1(TX)

19(RX), 18(TX)

17(RX), 16(TX)

15(RX), 14(TX)