Does there any module you have it that support read/ write RFID tag at one source code, in this moment I use two RFID modules one for read and other one for Write. If you have please mention the module or give me a link that available in Russia.
Hi there,
1. Please check if Grove-NFC meets your requirement. http://wiki.seeedstudio.com/Grove_NFC/
2. For the Russian distributor, you can refer to https://www.seeedstudio.com/distributors.html
Thanks
best rgds
Bill
Thanks
best rgds
Bill
It does not work with Arduino Mega 2560 R3, I did solid four pins for GNU VCC TX RX and connected with 20, 21 nothing? any idea!!
[cid:440097f9-a820-4c28-903e-7098771dc5e1]
Hi there,
We suggest UART(by default) to communicate with Mega. So you have to use the TX of NFC to RX of Mega(such as 19/17/15), and RX of NFC to TX of Meag(such as 18/16/14). thanks.
Thanks
best rgds
Bill
| BOARD | USB CDC NAME | SERIAL PINS | SERIAL1 PINS | SERIAL2 PINS | SERIAL3 PINS |
|---|---|---|---|---|---|
Uno, Nano, Mini |
0(RX), 1(TX) |
||||
Mega |
0(RX), 1(TX) |
19(RX), 18(TX) |
17(RX), 16(TX) |
15(RX), 14(TX) |
|
Thanks
best rgds
Bill