Distance from 40-pin header to top edge of the WIOT case

I’ve looked at the mechanical drawings for the WIO Terminal and don’t see the distance from the center of the 40-pin header to the top edge of the plastic case specified. Can someone from Seeed provide this from the mechanical drawing of the plastics, or could someone who already has received theirs already measure it for me?

thanks!
-eric

Hi @ericwertz
The distance from the center of the 40-pin header to the top edge of the plastic case is 13mm.

Hi,
Here’s a draft dimension drawing of the connector related to the case dimensions and the assembly threaded holes (extracted from the DXF). Image is a bit fuzzy, as SVG format is not allowed.
Tolerances are not known. Hope this helps.
heke++

This would be great to get into the wiki. I finally got mine a few days/weeks after my initial post and made the measurements that I needed.

This would be useful for anyone wanting to make their own accessory boards.

tkx!