Dimensions of the transparent cover for the ODYSSEY X86J4105

Hi,
I’m printing a replacement that includes a window for the status 2" LCD screen.
What are the official dimensions of that cover and what is the radius of the corners?

Maciej

@Maciej_Eckstein
files.seeedstudio.com/products/102110399/Documents/re_computer case.dxf

Link not working due to a missing space. The following link works for me:

https://files.seeedstudio.com/products/102110399/Documents/re_computer%20case.dxf

I measured the dimensions on the drawing and also measured the size of the cover itself.

Drawing: 117.1mm x 126.1mm
Cover: 116.8mm x 125.8mm

Cheers,

Leigh.

yep, I got that figured out already.


(cant attach an stl here )