I was looking at the LoRa-E5 Mini for a potential project and noticed that when I imported the Eagle pcb files into KiCad (6.0.2), the bottom two screw holes are not certainly aligned. Thought that was a bit strange.
Also, It would be nice if the Wiki had a PDF with the mechanical layout and dimensions of the board. I know there is the ruler image, but that is not really sufficient for somebody to make either a housing with or make a daughter-card such that the screw holes and breakout pins align.