Hello! I cant start use DepthEye 3D visual ToF Depth Camera on Raspbian.
Have tried different manuals but got segfault because of using ubuntu mate
libdeptheyeh1cdk.so ((((
Also I’ve tried to compile vortexsdk (with openni2/openni), but no luck,
binary tools cant see camera… ((
Please help!
Hi there,
Thanks
best rgds
Bill
Hi there,
We tested it with raspberry pi and it works well, so did our customer.

Please check below items.
3. Please use CMakeLists_ubuntu_mate.txt as CMakeLists.txt to replace the old one before you run "cmake .."
best rgds
Bill
Hi there,
Sensor Features:
Measures Phase with QVGA(80x60)resolution
1/6" Optical Format
Up to 1000fps frame rate
Global Reset & Shutter
-
Programmable Features
-Frame Size, frame rate
-Exposure, ROI
De-aliasing, temp compensation
IR pass filter (820nm to 865nm)
12-bit Phase/Amplitude, 4-bit Ambient
Parallel Operating Temperature:0°C to + 70°C
Thanks
best rgds
Bill
Ok, I got it… But can you help me please where to make changes for get
more than 30 fps (in Header files I see only 15/30 switch)
Thank you very much!
??, 15 ??? 2019 ?. ? 04:28, seeed_support [email protected]:
Ok, I got it… But can you help me please where to make changes for get
more than 30 fps (in Header files I see only 15/30 switch)
Thank you very much!
??, 15 ??? 2019 ?. ? 04:28, seeed_support [email protected]:
Hi there,
Thanks
best rgds
Bill
Thanks a lot! I will try.
??, 15 ??? 2019 ?. ? 13:15, seeed_support [email protected]:
I tried to change frame_rate parameter in conf file, and recompiled
H1AsciiSample program, but still see “30 fps” in start message ((( I’ve
found frame_rate parameter in voxel.so libs, but dont know how to recompile
it to apply new parameter. Can you give me some hints?
Thank you very much!
??, 15 ??? 2019 ?. ? 13:48, Sergey Skorchenko [email protected]:
When I change parameters in DepthEyeH1CDKCameraH1ForSeeed.conf,
H1AsciiSample starting and fps does not changed. When I removed this file,
sample program warnings about no config and starts with defaults 30 fps.
What should I do to apply any changes? Maybe some manual exists with rules
and restrictions of setting parameters in
DepthEyeH1CDKCameraH1ForSeeed.conf file?
Best regards!
??, 15 ??? 2019 ?. ? 13:57, Sergey Skorchenko [email protected]:
I think I’ve found how to change fps. Need to remove depthEyeSys.setMode
call in source code. Thank you!
??, 15 ??? 2019 ?. ? 14:21, Sergey Skorchenko [email protected]: