Debug environment for Himax WE2

I found the following toolchain for firmware development on Himax WE2 (Grove Vision AI v2):
:

Is any debugging environment also available for Himax WE2?

Hi there,

Check the following link:

As it’s suggested, CMSIS-DAP Compatible Debuggers should be able to work. Dev team confirmed that they used NXP Semicoductor MCU-LINK.

Thanks a lot, very interesting info!

Is this toolchain available only with Linux as a requirement?
Is it possible to do the same with Windows?

Short answer is, yes. Since both toolchain and pyOCD are supported on Windows, it’s fair to give it a try.

Build Firmware on Windows

Arm Toolchain Download Center - 13.2

pyOCD Guide

The link:

mentions a JTAG to SWD adapter.
What is the exact type (P/N) of this adapter?

It seems that we were unable to find the exact same one online, but similar one should work. Mainly a JTAG to SWD converter.

It is also my question why should we need an JTAG to SWD adapter at all, since the MCU-Link debug probe already provides SWD interface connector?

It is also my question why should we need an JTAG to SWD adapter at all, since the MCU-Link debug probe already provides SWD interface connector?