Are there any tutorials or support for building/updating the device tree for a different camera driver? I know Seeed provides the updated top level .dtb kernel for the A203 carrier board (thanks!) but as far as I can tell, I need to build the kernel from Nvidia source which would override the Seeed driver.
For clarity, I need a kernel driver and device tree (or overlay) to connect a MIPI camera to the CSI port on the A203v2 with an Nvidia Jetson TX2 NX module. I successfully flashed this setup and tested an 8mp IMX219 which is natively supported by the kernel. However, I need it to work with either an AR1335 (e-consystems e-CAM131_CUNX) or IMX477 (Arducam).