Hi,
I need clarification on CSI port and cable that should be used with jetson recomputer j3011board.
In the datasheet, I see it is 2 x 15 pin CSI port and the 15 pin FPC cable is fitting properly.
I have this i2c error between raspberry pi HQ camera and the jetson.
Most of the websites use 22 pin on jetson side to 15 pin connection on camera side.
Can you please clarify this?
I get this error even without camera connected which I don’t understand.