Corrupt Heap Error when trying to implement Edge Impulse TinyML into Xiao ESP32-S3

Hi, I’m quite new to using the Xiao ESP32-S3 module and wanted to try to learn how to implement TinyML to the module. I recently tried to follow the tutorial from Marcelo Rovai about implementing IMU sensors with the module.

However, when I tried to do this, I seem to be constantly getting the following error in the serial monitor:

CORRUPT HEAP: Bad tail at 0x3fcecec0. Expected 0xbaad5678 got 0x9dfd13b7

assert failed: multi_heap_free multi_heap_poisoning.c:276 (head != NULL)


Backtrace: 0x4037676e:0x3fceb2f0 0x4037b9b5:0x3fceb310 0x40380dfd:0x3fceb330 0x4037ff99:0x3fceb460 0x40377486:0x3fceb480 0x40380e55:0x3fceb4a0 0x4202286d:0x3fceb4c0 0x42021955:0x3fceb4e0 0x42007fc5:0x3fceb500 0x420062da:0x3fceb520 0x42006735:0x3fceb580 0x4200735e:0x3fceb630 0x4200759b:0x3fceb6d0 0x4200499b:0x3fceb700 0x42004add:0x3fceb790 0x42004cda:0x3fceb840 0x4200dcb5:0x3fcebe40

Does anyone know how this could be fixed? Here is the code I’m currently using:

/* Edge Impulse ingestion SDK
 * Copyright (c) 2022 EdgeImpulse Inc.
 *
 * Licensed under the Apache License, Version 2.0 (the "License");
 * you may not use this file except in compliance with the License.
 * You may obtain a copy of the License at
 * http://www.apache.org/licenses/LICENSE-2.0
 *
 * Unless required by applicable law or agreed to in writing, software
 * distributed under the License is distributed on an "AS IS" BASIS,
 * WITHOUT WARRANTIES OR CONDITIONS OF ANY KIND, either express or implied.
 * See the License for the specific language governing permissions and
 * limitations under the License.
 *
 */

/* Includes ---------------------------------------------------------------- */
#include <accelerometer_test_inferencing.h>
#include "I2Cdev.h"
#include "MPU6050.h"
#include "Wire.h"

/* Constant defines -------------------------------------------------------- */
MPU6050 imu;
int16_t ax, ay, az;

#define ACC_RANGE           1 // 0: -/+2G; 1: +/-4G
#define CONVERT_G_TO_MS2    (9.81/(16384/(1.+ACC_RANGE)))
#define MAX_ACCEPTED_RANGE  (2*9.81)+(2*9.81)*ACC_RANGE   

/*
 ** NOTE: If you run into TFLite arena allocation issue.
 **
 ** This may be due to may dynamic memory fragmentation.
 ** Try defining "-DEI_CLASSIFIER_ALLOCATION_STATIC" in boards.local.txt (create
 ** if it doesn't exist) and copy this file to
 ** `<ARDUINO_CORE_INSTALL_PATH>/arduino/hardware/<mbed_core>/<core_version>/`.
 **
 ** See
 ** (https://support.arduino.cc/hc/en-us/articles/360012076960-Where-are-the-installed-cores-located-)
 ** to find where Arduino installs cores on your machine.
 **
 ** If the problem persists then there's not enough memory for this model and application.
 */

/* Private variables ------------------------------------------------------- */
static bool debug_nn = false; // Set this to true to see e.g. features generated from the raw signal

/**
* @brief      Arduino setup function
*/
void setup()
{
    // put your setup code here, to run once:
    Serial.begin(115200);
    // comment out the below line to cancel the wait for USB connection (needed for native USB)
    while (!Serial);
    Serial.println("Edge Impulse Inferencing Demo");

    // initialize device
    Serial.println("Initializing I2C devices...");
    Wire.begin();
    imu.initialize();
    delay(10);

    //Set MCU 6050 OffSet Calibration 
    imu.setXAccelOffset(-4732);
    imu.setYAccelOffset(4703);
    imu.setZAccelOffset(8867);
    imu.setXGyroOffset(61);
    imu.setYGyroOffset(-73);
    imu.setZGyroOffset(35);

    imu.setFullScaleAccelRange(ACC_RANGE);

    if (EI_CLASSIFIER_RAW_SAMPLES_PER_FRAME != 3) {
        ei_printf("ERR: EI_CLASSIFIER_RAW_SAMPLES_PER_FRAME should be equal to 3 (the 3 sensor axes)\n");
        return;
    }
}

/**
 * @brief Return the sign of the number
 * 
 * @param number 
 * @return int 1 if positive (or 0) -1 if negative
 */
float ei_get_sign(float number) {
    return (number >= 0.0) ? 1.0 : -1.0;
}

/**
* @brief      Get data and run inferencing
*
* @param[in]  debug  Get debug info if true
*/
void loop()
{
    ei_printf("\nStarting inferencing in 2 seconds...\n");

    delay(2000);

    ei_printf("Sampling...\n");

    // Allocate a buffer here for the values we'll read from the IMU
    float buffer[EI_CLASSIFIER_DSP_INPUT_FRAME_SIZE] = { 0 };

    for (size_t ix = 0; ix < EI_CLASSIFIER_DSP_INPUT_FRAME_SIZE; ix += 3) {
        // Determine the next tick (and then sleep later)
        uint64_t next_tick = micros() + (EI_CLASSIFIER_INTERVAL_MS * 1000);

        imu.getAcceleration(&ax, &ay, &az);       
        buffer[ix + 0] = ax;
        buffer[ix + 1] = ay;
        buffer[ix + 2] = az;
       
        //ei_printf("raw values:    %.2f, %.2f, %.2f\n", ax*CONVERT_G_TO_MS2, ay*CONVERT_G_TO_MS2, az*CONVERT_G_TO_MS2);
        
        buffer[ix + 0] *= CONVERT_G_TO_MS2;
        buffer[ix + 1] *= CONVERT_G_TO_MS2;
        buffer[ix + 2] *= CONVERT_G_TO_MS2;

        for (int i = 0; i < 3; i++) {
            if (fabs(buffer[ix + i]) > MAX_ACCEPTED_RANGE) {
                buffer[ix + i] = ei_get_sign(buffer[ix + i]) * MAX_ACCEPTED_RANGE;
            }
        }

        delayMicroseconds(next_tick - micros());
    }

    // Turn the raw buffer in a signal which we can the classify
    signal_t signal;
    int err = numpy::signal_from_buffer(buffer, EI_CLASSIFIER_DSP_INPUT_FRAME_SIZE, &signal);
    if (err != 0) {
        ei_printf("Failed to create signal from buffer (%d)\n", err);
        return;
    }

    // Run the classifier
    ei_impulse_result_t result = { 0 };

    err = run_classifier(&signal, &result, debug_nn);
    if (err != EI_IMPULSE_OK) {
        ei_printf("ERR: Failed to run classifier (%d)\n", err);
        return;
    }

    // print the predictions
    ei_printf("Predictions ");
    ei_printf("(DSP: %d ms., Classification: %d ms., Anomaly: %d ms.)",
        result.timing.dsp, result.timing.classification, result.timing.anomaly);
    ei_printf(": \n");
    for (size_t ix = 0; ix < EI_CLASSIFIER_LABEL_COUNT; ix++) {
        ei_printf("    %s: %.5f\n", result.classification[ix].label, result.classification[ix].value);
    }
#if EI_CLASSIFIER_HAS_ANOMALY == 1
    ei_printf("    anomaly score: %.3f\n", result.anomaly);
#endif
}

#if !defined(EI_CLASSIFIER_SENSOR) || EI_CLASSIFIER_SENSOR != EI_CLASSIFIER_SENSOR_ACCELEROMETER
#error "Invalid model for current sensor"
#endif

Hi there,
Roll back the ESP32 b.s.p. to 2.14 afaik the alpha’s currently don’t work.
My .02
HTH
GL :slight_smile: PJ

Thank you for sharing your comment. I encountered difficulty locating the I2S Library while using version 3.0.2, but I managed to resolve it after roll back to 2.14.