Hello I recently purchased the Nvidia Jetson Orin, is it possible to interface it using this card ? (here is the link: DesignCore® NVIDIA® Jetson SerDes Sensor Interface Card | D3 Embedded )
Hi there,
Can you say more on Which Orin platform you have?
The D3 unit is for the High end "AGX " unit. " The NVIDIA® Jetson™ SerDes Sensor Interface card is an add-on for the NVIDIA Jetson AGX Orin™ and AGX Xavier™ Developer Kits. "
HTH
GL
PJ ![]()
Seed also sells a basic add on unit… Here I think? —> reServer Industrial J501-GMSL extension board
eServer Industrial J501-GMSL extension board
SKU
102991855
The J501 GMSL Extension Board is designed for J501 carrier board. You could use this extension to connect up to 8 GMSL camera. This carrier board is using the deserializer ‘max96724’. ![]()
The Nvidia Jetson Orin is a reComputer J30