Compatible wifi module for jetson orin nx 16gb

Hello

can anyone recommend any compatible wifi card or other solution for this one?

reComputer J4012-Edge AI Device with NVIDIA Jetson Orin™ NX 16GB module - Seeed Studio

thanks

Since the reComputer J4012-Edge AI Device likely has an M.2 slot for WiFi expansion, you can look for M.2 WiFi cards that are compatible with the Jetson Orin™ NX module. Some options include Intel WiFi 6 AX200, Intel Dual Band Wireless-AC 8265, or Qualcomm Atheros QCA9377. e.g: aim apps

Hi there,
I was surprised no "E-Key " M.2 slot …AX200 wow good choice.
GL :slight_smile: PJ :+1:

AX200 I can confirm that it works on Jetpack 5.1.1. On JP6 I still try to make it work

I use a TP-link range extender * ![TP-LINK TL-WA850RE Repetidor WiFi/ Amplificador 300Mbps](t as an ‘antenna’ for my J4012.
I connect the repeater to my wifi network and through a ethernet cable I connect it to J4012 and get IP.
I hope it is quite clear what I did, but if not, let me know and I will upload a photo of my ‘wifi’ external card through ethernet. this way you don’t need drivers for wifi and it just works.