Hello
How can I check if the firmware is good on my lipo rider pro ? and how reprogram it ?
Thanks
Hello
How can I check if the firmware is good on my lipo rider pro ? and how reprogram it ?
Thanks
er… 
a bit confused, i think their is no firmware for the lipo rider pro…
but I saw this on wiki :
If a firmware reprogram for the outdoor sensor device is required, simple connect the mini USB port to your PC which will put the device under “Program Mode” as explained above.
What does it means ?
Hey , maybe there are some misunderstanding you have got from our wiki. In fact , the “USB Mode” is just the charging mode, that means you can use the lipo rider pro to charge your outdoor devices. And the “Program Mode” has nothing to do with the firmware updating, that means you can connect the input to your PC, and connect the output to your devices(such as Arduino) , so you can upload the program to your devices via PC directly , and in this “Program Mode” you can regard lipo rider pro just as a “line conductor”.
Ohhhh

It explain every thing

Thanks ^^