Cannot flash Jetson Xaviar AGX H1

I am trying to flash Jetpack 5.0.2 to a Seeed Jetson AGX Xavier H01 Kit using the SDK Manager with Ubunutu 20.04 Host.
But flash process always fails at the very beginning with:
“000000003626050d: E> NV3P_SERVER: Could not read eeprom for module cvb.”

@Seeed: Should it be possible to flash the AGX with the SDK Manager in general? And with Jetpack 5.0.2. especially?

@Community: Has anyone else successfully flashed the device using SDKManager?

We recommend not using JetPack 5.0.2 yet, we don’t have a driver for this version yet, so stay tuned.

Thanks @Citric for the answer.

My other questions I can now answer myself and maybe the answer is helpful for others new to this area. It seems not to be possible to flash the AGX with SDK Manager. Instead you really have to do it with the flash.sh script.

Following the description in Seeed wiki and Readme.txt in downloaded 5.0.1 driver package from Seeed (only the folders are a bit different) I was able to flash Jetpack 5.0.1 to the Xavier without any issues.

What a coincidence, the driver is fresh out today! H01 already supports Jetpack 5.0.2!
505_jp5.0.2.zip (60.8 KB)