Cannot Change WiFi on Xiao 7.5 OG Running TRMNL

Greetings! I picked up the Xiao 7.5 OG screen (Assembled vs DIY – runs on the c3 not the s3). I had it delivered to work (porch pirates have been active), and I loaded the TRMNL firmware and set everything up without issue. Once I was satisfied that it was behaving properly, I took it home with the intent to re-enter provisioning mode and switch the wifi settings.

That was my intent, in any case, however I can not find any combination of button presses to expose the capture screen and allow me to change the wifi. I could reflash it, I suppose, but does anyone know how to get it to just re-enter provisioning so that I can enter the new network credentials?

Dave

Oh discord, what problems can you not solve? For the record, the answer is: Press the Reset button on the XIAO, release it, then press and hold the Boot button for five seconds

Hi. Have you got the Seeedstudio XIAO ePaper board? 'cos I got the same issue and I can’t reset it in any way. Tried as you said, but it just reboots and say wifi connected (at work). But I wanna bring it home.

Interesting as there is only the one firmware version available for it. Did you try just reflashing it at home? If reset followed by press and hold boot doesn’t work, their may be corruption. To be clear, though, this is the epaper panel (assembled) not the Xiao DIY Kit. They use different esp32 boards.