But After rebooting, when I connected to the screen with the HDMI cable, there is nothing coming on the screen. Can anyone give an idea on what has gone wrong here?
Hi there,
I have seen this issue pop up from time to time.
things like remove the coin cell battery after flash and reboot, ymmv
Search for NO HDMI and jetson, should get some links.
HTH
GL PJ
I have tried flashing multiple times, after removing extra hardware (Wifi adapter), but it still have the same issue. I realised the system is booting up, I could connect to it over SSH when the USB cable is connected to the host machine. And when I list the hardware in the system, nothing related to display is present. Is there a way to configure this?