Can i use the grove speech recognizer kit for arduino to make a lamp voice controlled

Can i use the grove speech recognizer kit for arduino to make a lamp voice controlled?

HI there You have to buy arduino and grove-relay(NOT included) to make the lamp controlled by voice.

<LINK_TEXT text=“https://www.seeedstudio.com/Seeeduino-L … -2896.html”>https://www.seeedstudio.com/Seeeduino-Lotus-Cortex-M0-p-2896.html</LINK_TEXT>



http://wiki.seeedstudio.com/Grove-Relay/

You can refer below voice command, for more info, please refer to http://wiki.seeedstudio.com/Grove-Speech_Recognizer/



Command

Value







Turn on the light

1





Turn off the light

2





Play music

3





Pause

4





Next

5





Previous

6





Up

7





Down

8





Turn on the TV

9





Turn off the TV

10





Increase temperature

11





Decrease temperature

12





What’s the time

13





Open the door

14





Close the door

15





Left

16





Right

17





Stop

18





Start

19





Mode 1

20





Mode 2

21





Go

22





thanksbest rgdsBill

Thank you, also are there any tutorials and codes for the grove relay? I’ve been looking online and can’t find anything
Sent from my iPhone

Hi there


You can check http://wiki.seeedstudio.com/Grove-Relay/ , it is digital signal.

Thanks

best rgds
Bill