I have followed the steps given in the following page: setup
This is the output I receive after using dmesg grep | spi:
[ 5.000330] mcp25xxfd spi1.0 (unnamed net_device) (uninitialized): Failed to detect MCP2517FD (osc=0x00000000).
[ 5.044938] mcp25xxfd spi0.0 can0: MCP2518FD rev0.0 (-RX_INT -MAB_NO_WARN +CRC_REG +CRC_RX +CRC_TX +ECC -HD m:20.00MHz r:18.50MHz e:0.00MHz) successfully initialized.
[ 5.053955] mcp25xxfd spi0.1 can1: MCP2518FD rev0.0 (-RX_INT -MAB_NO_WARN +CRC_REG +CRC_RX +CRC_TX +ECC -HD m:20.00MHz r:18.50MHz e:0.00MHz) successfully initialized.
[ 6.806591] spi_master spi1: will run message pump with realtime priority
[ 6.846089] mcp251xfd spi1.0 (unnamed net_device) (uninitialized): Failed to detect MCP2517FD (osc=0x00000000).