CAN-BUS monitor on 2012 GM V6

I purchased the CAN-BUS analyzer and loaded the driver and version 7.20 of the software. I’m connected to a 2012 GM 3.6L V6 ECU. The software show connection is good and status Bus-on. But no data is displayed in the tool.

Any help would be greatly appreciated.

For reference: I can connect and read data using HPTuners. It returns this information;
Protocol Info: ISO 15765-2, J1962: CAN, 500 kb/s
Scanning Methods: ISO 15031-5 Mode 0x01 Functional, ISO 15031-5 Mode 0x01 Physical, CAN Listener, SAE J2190 Mode 0x22, HPT Mode 0x23, GM Mode 0x2C 0x2D 0xAA