Can Bluetooth Bee be set to BTstate 1 (Ready) on startup?

I just want to verify whether or not the Bluetooth Bee module can be setup with AT commands to automatically be discoverable when powered on. It looks like it has to have a hardwired serial string “\r\n+INQ=0\r\n” sent each time it is turned on in order to be discoverable via Bluetooth (setup in slave mode). Thanks in advance,

Jeremy

Hi Jeremy,

There is a command(\r\n+STAUTO=1\r\n) which could enable the Bee auto-connect the last paired device when start up on the user manual.

With this command, the Bee will auto-connect to the last paired device, and you can only disconnect them by giving a rising pulse in PIO0.

May this helpful to you,

Regards,

-Icing

Icing,

Thanks for the quick reply. I may do a tutorial on using your module so I am glad to confirm that fact with you.

Regards,

Jeremy