Build projects for XIAO MG24 using SimplicityStudio

This is the continuation of the other thread about MG24 boards

@grobasoz

What would be the missing steps to add to the list?

Can we start with the assumption that Simplicity Studio 5 has been installed along with the relevant SiSDK (currently 2025.6.1)?

Or despite Simplicity Studio 6 being in Beta work with that? It supports VSCode as well… (Same SiSDK).

“We” can then build out the necessary steps to build a Matter device, viz Light, starting with “internal” bootloader and later using the “external” (SPI flash) bootloader for OTA?

Yes. Yes, I have it on my PC

OK

I will be building a Matter Light App (Internal Bootloader) for XIAO MG24 using Simplicity Studio 5 and SiSDK 2025.6.1.

Step 1.
Select the Launcher tab.

Step 2 & 3.
Add the XIAO MG24 chip (EFR32MG24B220F1536IM48) to the “My Products” section of Simplicity Studio.

Step 4.
Select Example Projects and Demos.

Step 5.
Filter on “light”

Step 6.
Select “Matter”

Step 7.
Select Matter - SoC Lighting over Thread with Internal Bootloader and click “Create”.

Final Step.
Select suitable names for Workspace, Bootloader and main Project (eg XIAO_MG24_MatterLight).

Adding some project details.

Step 1.
Once the project has been created, select the “Software Components” tab.

Step 2.
Filter on “Configurable” and “Installed”

Step3.
Select Platform → Driver → Led → Simple LED->inst0.

Step 4.
Click “Configure”.

Step 5.
Select “Active Low” polarity and PA07 as “Selected Module” then click X (Close).

Step 6.
Select the UART EUSART → vcom instance and click “Configure”.

Step 7.
Set the vcom settings as below… and click X.

Step 8.
In the “Project Explorer” select the project and Right Click → Build Project (or Click the “Hammer” button in the menu bar).

The project should build without errors.

Additional Settings for XIAO MG24.

Step 1.
Deselect “Installed” checkbox. (We’re adding new “components”).

Step 2.
Filter on “gpio”.

Step 3.
Select GPIO Init (from Platform->Peripheral->EMLIB->Init).

Step 4.
Click “Install”.

Step 5.
Choose and “Instance Name” - eg RF_PWR.

Step 6.
Click “Configure”.
(If the “No Entry” sign appears over the “Configure” button, wait a little bit…)

Step 7.
RF_PWR

  • Pin Mode - stays the same.
  • DOUT - 1
  • Selected Module is PB05
    X = Close.

Repeat this by clicking “+ Add New Instance” for…

  1. The RF_SW - Pin Mode (Same), DOUT (0), Selected Module (PB04).
  2. Any other GPIO required (or skip for now).

Build the project.

Programming and Debugging.

There are two options available for programming and debugging the XIAO MG24 projects.

  1. Via built in SWD via OpenOCD.
  2. Using the SWD pads and a Segger JLink (compatible) debugger.

Option 1.
Quite involved - will tackle this later.

Option 2.
Either solder SWD connections to the XIAO MG24 or use the Expansion Board to connect SWD to the device.
Only GND, SWDIO and SWCLK are required.

Select the “bootloader” project and build the project.
In the “Binaries” folder of the bootloader project, select the “hex” file and Right Click → Flash to Device.
Select your JLink connected to the XIAO MG24 and click OK.

Erase and Program the device.

Select the “light” project and click the “Debug” symbol on the menu bar (or Right Click → Debug As → 1 Silicon Labs ARM Program.

Select the JLink and click OK.
The Debug perspective will be opened and the code set at “sl_main_second_stage_init();” function.

Connect a Serial Terminal (eg PuTTY) to the XIAO MG24 serial port.
Click the run button to start the debugger.

The following messages are sent…

[00:00:00.125][info  ][DL] Starting scheduler
[00:00:00.125][info  ][DL] ==================================================
[00:00:00.126][info  ][DL] SL-Light starting
[00:00:00.126][info  ][DL] ==================================================
[00:00:00.126][info  ][DL] Init CHIP Stack
[00:00:00.131][info  ][DL] Setting device name to : "SL-Light"
[00:00:00.132][info  ][DL] Provision mode disabled
[00:00:00.132][info  ][DL] Initializing OpenThread stack
[00:00:00.133][info  ][DL] OpenThread started: OK
[00:00:00.134][info  ][DL] Setting OpenThread device type to ROUTER
[00:00:00.134][info  ][DL] Starting OpenThread task
[00:00:00.135][info  ][SVR] Initializing subscription resumption storage...
[00:00:00.137][info  ][SVR] Server initializing...
[00:00:00.137][detail][FP] Initializing FabricTable from persistent storage
[00:00:00.138][info  ][TS] Last Known Good Time: [unknown]
[00:00:00.138][info  ][TS] Setting Last Known Good Time to firmware build time 2                                  023-10-10T16:28:52
[00:00:00.140][info  ][DMG] AccessControl: initializing
[00:00:00.141][info  ][DMG] Examples::AccessControlDelegate::Init
[00:00:00.141][info  ][DMG] AccessControl: setting
[00:00:00.141][info  ][DMG] DefaultAclStorage: initializing
[00:00:00.142][info  ][DMG] DefaultAclStorage: 0 entries loaded
[00:00:00.142][info  ][SVR] WARNING: mTestEventTriggerDelegate is null
[00:00:00.142][detail][IN] UDP::Init bind&listen port=5540
[00:00:00.143][detail][IN] UDP::Init bound to port=5540
[00:00:00.143][detail][IN] BLEBase::Init - setting/overriding transport
[00:00:00.143][detail][IN] TransportMgr initialized
[00:00:00.148][detail][DL] Using Thread extended MAC for hostname.
[00:00:00.150][info  ][ZCL] Using ZAP configuration...
[00:00:00.151][detail][DMG] Failed to read stored attribute (0, 0x0000_0028, 0x0                                  000_0005: a0
[00:00:00.152][detail][DMG] Failed to read stored attribute (0, 0x0000_0028, 0x0                                  000_0010: a0
[00:00:00.154][detail][DMG] Failed to read stored attribute (1, 0x0000_0006, 0x0                                  000_0000: a0
[00:00:00.155][detail][DMG] Failed to read stored attribute (1, 0x0000_0006, 0x0                                  000_4003: a0
[00:00:00.156][detail][DMG] Failed to read stored attribute (1, 0x0000_0008, 0x0                                  000_0000: a0
[00:00:00.157][detail][DMG] Failed to read stored attribute (1, 0x0000_0008, 0x0                                  000_4000: a0
[00:00:00.158][detail][DMG] Failed to read stored attribute (1, 0x0000_0300, 0x0                                  000_0000: a0
[00:00:00.159][detail][DMG] Failed to read stored attribute (1, 0x0000_0300, 0x0                                  000_0001: a0
[00:00:00.160][detail][DMG] Failed to read stored attribute (1, 0x0000_0300, 0x0                                  000_0003: a0
[00:00:00.161][detail][DMG] Failed to read stored attribute (1, 0x0000_0300, 0x0                                  000_0004: a0
[00:00:00.162][detail][DMG] Failed to read stored attribute (1, 0x0000_0300, 0x0                                  000_0007: a0
[00:00:00.163][detail][DMG] Failed to read stored attribute (1, 0x0000_0300, 0x0                                  000_0008: a0
[00:00:00.164][detail][DMG] Failed to read stored attribute (1, 0x0000_0300, 0x0                                  000_4000: a0
[00:00:00.165][detail][DMG] Failed to read stored attribute (1, 0x0000_0300, 0x0                                  000_4001: a0
[00:00:00.166][detail][DMG] Failed to read stored attribute (1, 0x0000_0300, 0x0                                  000_4002: a0
[00:00:00.166][detail][DMG] Failed to read stored attribute (1, 0x0000_0300, 0x0                                  000_4003: a0
[00:00:00.166][detail][DMG] Failed to read stored attribute (1, 0x0000_0300, 0x0                                  000_4004: a0
[00:00:00.168][detail][DMG] Failed to read stored attribute (1, 0x0000_0300, 0x0                                  000_4010: a0
[00:00:00.168][info  ][DMG] AccessControlCluster: initializing
[00:00:00.168][detail][ZCL] GeneralDiagnostics: OnDeviceReboot
[00:00:00.169][detail][DMG] Endpoint 0, Cluster 0x0000_0033 update version to d3                                  5a9324
[00:00:00.169][detail][EVL] LogEvent event number: 0x0000000000000000 priority:                                   2, endpoint id:  0x0 cluster id: 0x0000_0033 event id: 0x3 Epoch timestamp: 0x00                                  0000DC6ACFAC28
[00:00:00.170][info  ][ZCL] Initiating Admin Commissioning cluster.
[00:00:00.170][detail][DMG] Endpoint 1, Cluster 0x0000_0003 update version to e2                                  afd74a
[00:00:00.171][info  ][ZCL] Cluster callback: 0x0000_0003
[00:00:00.171][info  ][ZCL] Identify attribute ID: 0x0000_0001 Type: 48 Value: 2                                  , length 1
[00:00:00.172][detail][DMG] Endpoint 1, Cluster 0x0000_0004 update version to b8                                  d0002f
[00:00:00.172][info  ][ZCL] Cluster callback: 0x0000_0004
[00:00:00.172][detail][DMG] Endpoint 1, Cluster 0x0000_0004 update version to b8                                  d00030
[00:00:00.173][info  ][ZCL] Cluster callback: 0x0000_0004
[00:00:00.173][info  ][ZCL] Endpoint 1 On/off already set to new value
[00:00:00.174][detail][DMG] Endpoint 1, Cluster 0x0000_0008 update version to c2                                  cfaab
[00:00:00.174][detail][DMG] Endpoint 1, Cluster 0x0000_0062 update version to fa                                  bd4a
[00:00:00.174][info  ][ZCL] Cluster callback: 0x0000_0062
[00:00:00.175][detail][DMG] Endpoint 1, Cluster 0x0000_0300 update version to a3                                  af4a7b
[00:00:00.176][detail][DMG] Endpoint 1, Cluster 0x0000_0300 update version to a3                                  af4a7c
[00:00:00.177][info  ][ZCL] Cluster callback: 0x0000_0300
[00:00:00.177][info  ][ZCL] Color Control attribute ID: 0x0000_0008 Type: 48 Val                                  ue: 2, length 1
[00:00:00.179][detail][DMG] Endpoint 1, Cluster 0x0000_0300 update version to a3                                  af4a7d
[00:00:00.179][info  ][ZCL] Cluster callback: 0x0000_0300
[00:00:00.179][info  ][ZCL] Color Control attribute ID: 0x0000_4001 Type: 48 Val                                  ue: 2, length 1
[00:00:00.181][detail][IN] SecureSession[0x20007920]: Allocated Type:1 LSID:6300                                  5
[00:00:00.182][detail][SC] Assigned local session key ID 63005
[00:00:00.182][detail][SC] Waiting for PBKDF param request
[00:00:00.182][info  ][DIS] Updating services using commissioning mode 1
[00:00:00.183][error ][DIS] Failed to remove advertised services: 3
[00:00:00.183][detail][DL] Using Thread extended MAC for hostname.
[00:00:00.184][info  ][DIS] Advertise commission parameter vendorID=65521 produc                                  tID=32773 discriminator=3840/15 cm=1 cp=0
[00:00:00.184][error ][DIS] Failed to advertise commissionable node: 3
[00:00:00.184][error ][DIS] Failed to finalize service update: 3
[00:00:00.185][info  ][DIS] Updating services using commissioning mode 1
[00:00:00.185][error ][DIS] Failed to remove advertised services: 3
[00:00:00.185][detail][DL] Using Thread extended MAC for hostname.
[00:00:00.186][info  ][DIS] Advertise commission parameter vendorID=65521 produc                                  tID=32773 discriminator=3840/15 cm=1 cp=0
[00:00:00.186][error ][DIS] Failed to advertise commissionable node: 3
[00:00:00.187][error ][DIS] Failed to finalize service update: 3
[00:00:00.187][info  ][IN] CASE Server enabling CASE session setups
[00:00:00.188][detail][IN] SecureSession[0x200079f8]: Allocated Type:2 LSID:6300                                  6
[00:00:00.188][detail][SC] Allocated SecureSession (0x200079f8) - waiting for Si                                  gma1 msg
[00:00:00.188][detail][ZCL] Emitting StartUp event
[00:00:00.189][detail][EVL] LogEvent event number: 0x0000000000000001 priority:                                   2, endpoint id:  0x0 cluster id: 0x0000_0028 event id: 0x0 Epoch timestamp: 0x00                                  0000DC6ACFAC3B
[00:00:00.189][info  ][SVR] Server Listening...
[00:00:00.190][silabs ]Starting Platform Manager Event Loop
[00:00:00.192][info  ][DL] Starting App Task
[00:00:00.475][info  ][DL] Bluetooth stack booted: v10.1.0-b0
[00:00:00.475][info  ][DL] RAIL version:, v2.19.1-b0
[00:00:00.476][detail][DL] CHIP event task running
[00:00:00.476][detail][DL] Start BLE advertisement
[00:00:00.477][detail][DL] BLE Static Device Address DF:4D:F2:55:30:71
[00:00:00.478][info  ][DL] Starting advertising with interval_min=32, intverval_                                  max=96 (units of 625us)
[00:00:00.480][info  ][DL] _OnPlatformEvent default:  event->Type = 32781
[00:00:00.481][info  ][DL] _OnPlatformEvent default:  event->Type = 32779
[00:00:00.482][detail][DL] OpenThread State Changed (Flags: 0x00038210)
[00:00:00.483][detail][DL]    Network Name: OpenThread
[00:00:00.483][detail][DL]    PAN Id: 0xFFFF
[00:00:00.483][detail][DL]    Extended PAN Id: 0xDEAD00BEEF00CAFE
[00:00:00.484][detail][DL]    Channel: 11
[00:00:00.484][detail][DL]    Mesh Prefix: fdde:ad00:beef:0:0:0:0:0/64
[00:00:00.485][info  ][SVR] Current Software Version String: 1
[00:00:00.485][info  ][SVR] Current Software Version: 1
[00:00:00.485][info  ][DL] Device Configuration:
[00:00:00.486][info  ][DL]   Serial Number: (not set)
[00:00:00.486][info  ][DL]   Vendor Id: 65521 (0xFFF1)
[00:00:00.487][info  ][DL]   Product Id: 32773 (0x8005)
[00:00:00.487][info  ][DL]   Product Name: SL_Sample
[00:00:00.488][info  ][DL]   Hardware Version: 1
[00:00:00.488][info  ][DL]   Setup Pin Code (0 for UNKNOWN/ERROR): 0
[00:00:00.488][info  ][DL]   Setup Discriminator (0xFFFF for UNKNOWN/ERROR): 384                                  0 (0xF00)
[00:00:00.489][info  ][DL]   Manufacturing Date: (not set)
[00:00:00.489][info  ][DL]   Device Type: 65535 (0xFFFF)
[00:00:00.490][info  ][SVR] SetupQRCode: [MT:6FCJ142C00KA0648G00]
[00:00:00.490][info  ][SVR] Copy/paste the below URL in a browser to see the QR                                   Code:
[00:00:00.490][info  ][SVR] https://project-chip.github.io/connectedhomeip/qrcod                                  e.html?data=MT%3A6FCJ142C00KA0648G00
[00:00:00.491][info  ][ZCL] On/Off ep1 value: 0
[00:00:00.491][silabs ]App Task started
matterCli> [00:00:30.481][info  ][DL] Starting advertising with interval_min=240, intverval_max=1920 (units of 625us)

Connecting to the Matter fabric (network).

From the matterCLI messages select the QRCode URL.

https://project-chip.github.io/connectedhomeip/qrcode.html?data=MT%3A6FCJ142C00KA0648G00

Get the QRCode and using your mobile phone and a suitable Matter device, add your new XIAO MG24 Light to your Matter network.

The XIAO MG24 On-Board LED will be affected by the Matter Device On/Off changes.

Thanks a lot man @grobasoz.

Just a little thing. There is a typo here. It should be EFR32MG24B220F1536IM48 like describe here, right?

Thanks for that - Fixed the typo :slight_smile:

Building light project seems OK:

Building target: XIAO_MG24_MatterLightOverThread.axf
Invoking: GNU ARM C++ Linker
arm-none-eabi-g++ '@XIAO_MG24_MatterLightOverThread.axf.rsp' -o XIAO_MG24_MatterLightOverThread.axf 
Finished building target: XIAO_MG24_MatterLightOverThread.axf
 
Building out file: XIAO_MG24_MatterLightOverThread.out
arm-none-eabi-objcopy "XIAO_MG24_MatterLightOverThread.axf" "XIAO_MG24_MatterLightOverThread.out"
 
Building hex file: XIAO_MG24_MatterLightOverThread.hex
arm-none-eabi-objcopy -O ihex "XIAO_MG24_MatterLightOverThread.axf" "XIAO_MG24_MatterLightOverThread.hex"
 
Building bin file: XIAO_MG24_MatterLightOverThread.bin
arm-none-eabi-objcopy -O binary "XIAO_MG24_MatterLightOverThread.axf" "XIAO_MG24_MatterLightOverThread.bin"
 
Building s37 file: XIAO_MG24_MatterLightOverThread.s37
arm-none-eabi-objcopy -O srec "XIAO_MG24_MatterLightOverThread.axf" "XIAO_MG24_MatterLightOverThread.s37"
 
Running size tool
arm-none-eabi-size "XIAO_MG24_MatterLightOverThread.axf" -A
XIAO_MG24_MatterLightOverThread.axf  :
section                    size        addr
.text                    894872   134242304
.ARM.exidx                    8   135137176
.copy.table                  12   135137184
.zero.table                   0   135137196
.stack                     4608   536870912
.data                      5780   536875520
.bss                     187976   536881300
text_application_ram          0   537069276
.heap                      2048   537069280
.nvm                      40960   135137196
.ARM.attributes              54           0
.comment                     69           0
.debug_line_str            2820           0
.debug_info            55057748           0
.debug_abbrev           1847527           0
.debug_aranges           154464           0
.debug_line             4570248           0
.debug_str              6072923           0
.debug_loc              4698248           0
.debug_ranges            572752           0
.debug_frame             505252           0
.debug_loclists           97132           0
.debug_rnglists           25084           0
Total                  74740585

So if I want to add a Button,do I have to install “Simple Button” like this and define the GPIO?

I am not sure about the mode:

You can use the “interrupt” mode.

Is there a way to disable matterCli and send the logs to the serial console instead of to debug?

Using the SWD pads and a Segger JLink (compatible) debugger seems to be an expensive approach with Segger debugger costing over $1,000.
Is there a lower cost compatible option to perform imaging of a project build using Simplicity as I would like to build Zigbee using the low power mg24 - arduino does not have libraries built for zigbee for this soc.

You can use the built in OpenOCD SWD interface (over the USB connection) for programming and debugging the XIAO MG24.
So, no need for (an expensive) Segger JLink.
A (relatively) cheap alternative to the Segger JLink is the Silicon Labs DBG1015A.

Hi @grobasoz, how can I flash a project that has a separate bootloader? In other words, how can I flash a project that’s external bootloader?

Another question: once I’ve compiled and flashed the project on the Xiaomi MG24, how do I put it into commissioning mode? Is it automatic? Because I’ve tried commissioning it in Home Assistant and it can’t find the device.

When I meant Xiaomi MG24, I actually meant XIAO MG24.

@grobasoz i don’t have a Segger JLink debugger, nor the Silicon Labs DBG1015A. I’m flashing with OpenOCD through USB, so I can’t see the log messages. I only see the MatterCLI commands. Is there any way to disable the MatterCLI commands and see the debug messages through USB?

Which project did you use?
If a Matter project, you can commission via the CLI or (in some cases) the buttons.

Hi @grobasoz, i’ve been using the Light project. I assume that when you say to use CLI commands, you specifically mean the command “ble adv start” to initiate Bluetooth commissioning. However, I haven’t been able to commissioner the project because, for some reason I don’t understand, it doesn’t finish commissioning the Matter device on my Thread network, where I use a Silabs border router dongle to commission Matter devices in Home Assistant. I’ve already commissioned several devices I’ve developed with Espressif’s ESP32, but I can’t get it to work with the Xiaomi MG24 device.

Thanks